Download (D4000206)

Issue Date : Oct.05.16

Category : Evaluation Software, IDE Upgrades

e² studio 5.2.0.020 installer (Offline installer)

Description

  • Click below for detailed information.

    This installer is capable of doing offline installation with included eclipse modules.
    You can also choose "Web Installer" from here if an Internet connection is available.

 

How to install

Please download the installer file from the "Download Link" shown below, then launch the installer.

Note 1: e² studio has no capability of updating from V4.3 or earlier versions to V5.0 or later including V5.2 .
Please uninstall the earlier versions before installation.
Alternatively, if you would like to keep an earlier installations, please create a new folder for the new installation.
Note 2: Compiler product downloads will be skipped with no Internet connection.
Note 3: Windows OS may display a warning message "This program might not have installed correctly" after installations have done. This message does not mean installation failure. Please dismiss the message box by choosing "This program installed correctly".

 

  • Windows® 10 (32-bit, 64-bit)
  • Windows® 8.1 (32-bit, 64-bit)
  • Windows® 7 (32-bit, 64-bit)

 

Download

Product Name File Name File Size Download Link
e² studio 5.2.0.020 installer (Offline installer) setup_e2_studio_5_2_0_020.exe 919.08 MByte
Back to Top
Contact