1. Home
    2. Promotions

Win a RX231 Wi-Fi Cloud Connectivity Kit

Enter to Win an RX231 Wi-Fi Cloud Connectivity Kit

The RX231 Wi-Fi Cloud Connectivity Kit provides an easy-to-use platform for connecting to the cloud and evaluating IoT solutions requiring Wi-Fi. The kit offers free connectivity to Renesas IoT Sandbox and is powered by Medium One’s IoT Data Intelligence Platform. This device is a hybrid MCU/DSP, providing superb MCU performance, low power consumption and power signal-processing capabilities.

The YWIRELESS-RX231 Wi-Fi Cloud Connectivity Kit includes:

  • 54 MHz RX231 MCU board with four Pmod connectors and E1/E2 Lite header for J-Link support
  • GT202 Wi-Fi module with Qualcomm QCA4002 low-energy Wi-Fi 802.11a/b/g/n SoC
  • Pmod-mounted 3-axis MEMS accelerometer: Analog Devices ADXL362
  • Arduino Shield Socket
  • USB Type B connector for power and USB 2.0 device interface (with cable)
  • Pre-programmed with Medium One’s Vibration Monitoring demo and Intrinsic ID’s IoT
  • Authentication demo based on their unique PUF technology
  • Free Renesas IoT Sandbox Cloud account

 

Fill out the form for your chance to win an RX231 Wi-Fi Cloud Connectivity Kit.

E-mail address must be a valid company e-mail address. Registrations with e-mails such as Gmail, Yahoo, etc. will not be processed.

Required fields are marked with an asterisk. (*)

Contact