1. Home
    2. Promotions

WIN A RENESAS OKTOBERFEST COASTER

Celebrate Oktoberfest with Renesas and Intersil and enter to win an exclusive beverage coaster

Intersil Oktoberfest Coaster

The beverage coaster is the first reference design created by Renesas and Intersil together and showcases a diverse portfolio of products for broad market applications. It consists of a self-contained PCB board inside a plastic casing to protect it from accidental spills, and features a Renesas Synergy™ Platform S3-series MCU, plus multiple power/analog components from the Intersil product line.


As a beverage approaches the coaster’s center, the LEDs blink with increasing frequency until the drink is set down on top. A TE Connectivity thermistor indicates if it is too warm (flashes red) or just right (flashes blue) while “The Chicken Dance” plays in the background.


This promotion has ended.

Contact