Install Icon

To start developing using the Synergy Platform, the Synergy Software Package and development tools will need to be installed on your computer. You could also install some optional specialized software add-ons, libraries, debugging utilities, and other tools depending on your requirements.

Sign in to My Renesas

To download software and tools, you will be required to sign in to your My Renesas account. If you do not have an account, please sign up for one.

Downloading and Installing the Synergy Software Package and Development Tools (Required)

Visit the Synergy Software Package page. Select and download one of the three options to install the following:

  • SSP platform installer with e2 studio – Installs the Synergy Software Package and eclipse-based e2 studio integrated development environment.
  • SSP standalone installer – Installs the Synergy Software Package only.
  • SSC standalone installer – Installs the Synergy Standalone Configurator.

Useful Tips

We recommend that new users use the "Quick Install" option provided in the installation wizard, to minimize the amount of manual configuration needed. You can always come back and install additional options later.

The platform installer includes the Synergy Software Package as well as the e2 studio development tool. There is no need to install this package separately.

For your reference, the Synergy Software Package user manual is also included in the platform installer.

Downloading and Installing Additional Software Add-ons and Debugging Utilities (Optional)

You can download additional software libraries, stacks and more from the verified software add-ons and SSP supplemental add-ons pages if your application requires specialized software functionality.

Documentation

Type Title Date
Manual - Software PDF 95.11 MB
Manual - Software ZIP 77.08 MB
Release Note PDF 1.04 MB
Quick Start Guide PDF 4.15 MB 日本語
Guide PDF 912 KB
Quick Start Guide PDF 2.49 MB 日本語
Guide PDF 404 KB
Release Note PDF 428 KB
Release Note PDF 248 KB
9 items