Applilet EZ PL is a programming software that can create microcontroller application software easily in a manner similar to solving a puzzle, without using any programming language.
This software allows even users who are unfamiliar with programming languages and do not have knowledge of software development to easily create a variety of microcontroller application software using a graphical user interface (GUI) on a host machine. Applilet EZ PL can also be used to study and evaluate the basic operation of a system that uses a microcontroller.
The system configuration for using Applilet EZ PL is shown below.
Host machine operating environment | |
---|---|
Supported operating systems | Windows 2000, Windows XP* |
CPU | Intel Pentium 300 MHz or higher |
RAM | 128 MB or more |
*Notes
In Applilet EZ PL, software can easily be generated using the following procedure.
In Applilet EZ PL, the GUI contains programming elements that have been broken down into small modules called "panels". Software can be generated automatically through logical combination of these panels.
The panels shown above are examples.
Sunhayato Corp. offers the following evaluation boards that allow users to easily try using Applilet EZ PL.
This is the download page for the Applilet EZ PL, a simple visual programming software.
It is assumed that customers who view or download any of the tools or materials shown on this and subsequent pages have agreed to the terms of the License Agreement.
Be sure to read the License Agreement before viewing or downloading these tools.
* You must agree to these terms before using any of the tools shown below.
Product name | Download | User's manual | Remarks |
---|---|---|---|
Applilet EZ PL V3.8 (program only) |
ZIP (5.58 MB) |
Applilet(R) EZ PL For Ver. 3.6 or Later (PDF | English, 日本語) (5.14 MB) |
NO |
Other tools need to be installed to edit source files generated by Applilet EZ PL in an integrated development environment and generate object files.
DF780547 | Device files for the 78K0/Kx2. Information for each product's memory and peripheral functions is included. Required for compiling/assembling. |
RA78K0 | An assembler supporting the 78K0/Kx2. There is a 32 KB code size restriction. The PM+ integrated development environment is included. |
CC78K0 | A compiler supporting the 78K0/Kx2. |
PRM78F0547 | Files necessary for writing a program to the flash memory. Information for writing to flash for each product (including the 78K0/KE2) is included. Required for the flash memory programmer GUI (Renesas Flash Programmer). |
SM+ for 78K0/KX2 | A software simulator for 78K0/Kx2. Allows programs to be debugged without using special hardware on the computer. |
Applilet | A tool that automatically generates programs for initial settings or controlling peripheral functions (timers, UART, A/D) of a microcontroller using the settings of a GUI. For details on Applilet, please see here. |
Renesas Flash Programmer | A GUI for flash memory programming for the 78K0/KX2. |
Where to obtain software:
RA78K0S | An assembler supporting the 78K0S/Kx1+. There is a 32 KB code size restriction. The PM+ integrated development environment is included. |
CC78K0S | A compiler supporting the 78K0S/Kx1+. |
DF789234 | Device files for the 78K0S/Kx1+. Information for each product's memory and peripheral functions is included. Required for compiling/assembling. |
PRM78F9234 | Files necessary for writing a program to the flash memory. Information for writing to flash for each product is included. Required for the flash memory programmer GUI. |
SM+ for 78K0S/Kx1+ | A software simulator for the 78K0S/Kx1+. Allows programs to be debugged without using special hardware on the computer. |
Applilet | A tool that automatically generates programs for initial settings or controlling peripheral functions (timers, UART, A/D) of a microcontroller using the settings of a GUI. For details on Applilet, please see here. |
Programmers | For 78K0S/Kx1+ flash programming, please use the MINICUBE2 and QB-Programmer, or the programming GUI that comes with the evaluation board. |
Where to obtain software: