1. Home
    2. Software and Tools
    3. Boards and Kits

Renesas Synergy™ AE-WI-FI Application Example for Wi-Fi Connectivity

The Renesas Synergy™ Application Examples for Wi-Fi Connectivity (AE-WiFi) provide a quick and easy path to add Wi-Fi connectivity to a variety of Synergy Platform Development Kits, Starter Kits, and Target Boards by utilizing the Wi-Fi Framework included in the Synergy Software Package (SSP).

 

Source projects for these examples are available for download from the Renesas SynergyTM Gallery located under the Partner Showcase section.

AE-Wi-Fi1

Kit Contents

  • PMOD: Wireless Network Interface (GT202)

 

Kit Features

  • Longsys GT202 module with SPI using PMOD connector
  • Compatible with most Synergy DKs, SKs, and TBs
  • Supported by the Renesas Synergy Software Package with Wi-Fi Framework
  • Come with 1 application project and 3 partner projects to help you get started quickly

 

Ordering Information

  • Ordering part number: YSAEWIFI-1
  • Box contents: Longsys GT202 module
  • Order online: coming soon!

 

Getting Started

Option A: Start using the application project (no could connectivity)

You will need a Synergy Platform Starter Kit SK-S7G2.

 

  1. Download the “Synergy Wi-Fi Application Project for SK-S7G2 - Application Project” from here. You will be asked to login using MyRenesas account. The application project folder includes the following:
  • Application project interactive board display with GUIX and demonstrates the features of the           Wireless Framework for the Synergy SSP.
  • Application note - Synergy Wi-Fi Application Project for SK-S7G2.
  • Application note - Importing a Renesas Synergy Project.

2. Follow the instructions in the application note - Synergy Wi-Fi Application Project for SK-S7G2.

 

Option B: Start with one of the three partner projects to add cloud connectivity using Renesas IoT Sandbox

You will need a Synergy Platform Starter Kit SK-S7G2 and have to register on the Synergy Gallery.

 

AE-WiFi1 based LED Toggle - Partner Project

1)  Download the partner project from here.

2)  Visit the step by step instructions here.

 

AE-WiFi1 based Heartbeat - Partner Project

1)  Download the partner project from here.

2)  Visit the step by step instructions here.

 

AE-WiFi1 based Proximity Sensor with Presence Analytics - Partner Project (requires a MaxSonar ultrasonic sensor)

1)  Download the partner project from here.

2)  Visit the step by step instructions here.

 

Useful Information

 

 

 

Below you will find information to support the development of your application.

 

Information supporting development tools

Title Description
My Renesas Create a My Renesas account to use our tool download services,receive e-newsletter/update notifications, and take advantage of our other services.
e-learning Information for studying and learning about microcontrollers and microprocessors.
FAQ Frequently asked questions and useful hints for development.
Forum A forum and community site to share technical information,
questions and opinions with others who use Renesas MCU's.
Tool News Tool release information and other important information.
Operating Environment Information on system requirements and operating environment for the latest version of tools.
Tool Environmental Information Information on RoHS compliance of tools.
Info on Discontinued Products A list of Renesas software and tools that have been discontinued and are no longer being offered for new projects.

Confirm below disclaimers

Input Renesas account name and password

You can filter the sample codes and application notes that are displayed using the below filters.

Confirm below disclaimers

Input Renesas account name and password

Menu
Contact