1. Home
    2. Press Center
    3. News Archive
    4. 2013
    5. Renesas Electronics Develops and Supplies Multi-Format Video Codec Hardware IP that Supports Low-Delay Processing
Stock Price
Investor Relations

Product Specifications of New Hardware IP

  • Supported standards

     Encode:

H.264/AVC HP@L4.2, MP@L4.2 and Constrained BP@L3

H.264/MVC Stereo HP@L4.1

MPEG-2 MP@HL

MPEG-4 SP@L6 and ASP@L5

H.263 BP@L70

WebM VP8

     Decode:

H.264/AVC HP@L4.2, MP@L4.2 and Constrained BP@L3

H.264/MVC Stereo HP@L4.1

MPEG-2 MP@HL

MPEG-4 SP@L6 and ASP@L5

H.263 BP@L70 and Profile3@L70

VC-1 SP@ML, MP@HL and AP@L3

AVS Jizhun@L6.2

Sorenson Spark

DivX® HD1080 profile

On2 VP6

WebM VP8

RealVideo® 8, 9 and 10

 

  • Resolution and Performance

    Supports up to 1920x1080 pixel resolutions

    1080p30 decoding or encoding @ 130 MHz

    1080p60 decoding or encoding @ 260 MHz

 

  • Achieves a 1 ms minimum processing delay

 

  • Interface

    AMBA 32-bit APB for communication with a host processor

    AMBA 128-bit AXI for the external memory

 

(Remarks)
DivX is a trademark or registered trademark of LLC, a subsidiary of Rovi Corporation. DivX is a trademark or registered trademark of RealNetworks, Inc. All other product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Contact