Can’t attend live? Register anyway, and we’ll send you a link to the slides and a video of the webinar when it’s finished.
In this free, 60-minute webinar, Dr.-Ing. Adam Korbel of Renesas explains how to support new automotive E/E architectures with dedicated “winning combo” chipset solutions.
The expert will also present a reference design that includes digital and analog Renesas ICs and comes with a reference software environment to enable an easy prototyping start.
Key topics and takeaways:
- Understand new automotive E/E architecture trends
- Discover the Renesas digital and analog chipset solution for Central Gateway/Connected
Gateway/High-performance-computer (HPC)/Car Server applications
- Learn how Renesas realizes the winning combo chipset approach on their evaluation boards and reference designs
- Find out how to reduce efforts on software development with the Renesas reference software environment
In this free, 60-minute webinar, Guanyuan Chen of Renesas explains how to combine an inductive position sensor (IPS) with an xEV inverter solution to reduce costs and the bill of materials (BOM) when compared to using a resolver.
Chengzhe Li will explain how the xEV inverter application model and software control the motor, reducing software development time and effort.
Key topics and takeaways:
Learn how to reduce BOM components by using IPS, which is 30% less expensive than resolvers
Find out how to save time when achieving noise immunity by utilizing a pre-verified high voltage inverter environment (400V, 100kW, 500Arms)
Discover how to reduce potential rework through simulation at the design stage by using sample application IGBT models
Learn how to reduce application software programming effort by automatically generating sample application software
Find out how to reduce driver software programming effort using driver software whose operation has been confirmed on the reference board
In this webinar you will learn:
• Types of applications that can most benefit from the combination of Panthronics NFC ICs and Renesas RA MCUs
• Details on IoT card readers, Point of Sale terminals, and wireless charging use cases
• How to use Renesas Winning Combination reference designs, Quick-Connect IoT Pmods and Panthronics Pmod expansion boards, which can significantly reduce your development time
• How to enable a secure NFC application in the shortest amount of time for numerous cost sensitive consumer and robust industrial applications
In this webinar, viewers will learn how easily a manufacturer can empower its devices with the DLMS protocol using Terranova's Smart Meter Library. DLMS / COSEM (IEC 62056, AINSI C12, EN13757-1) is the global standard for energy and water smart management, advanced control, and innovative metering.
Webinar topics:
- Analyze key features of the product
- Examine the technical benefits and overall architecture
- Highlight the RA and RL78 platform support
In this webinar, you will learn:
- What O-RAN is and its advantages over traditional RAN topologies
- Timing topologies and requirements for each of the four synchronization plane configuration modes as defined by the O-RAN Alliance
- How Renesas' complete HW and SW timing solutions, with ClockMatrix hardware and PCM4L software, meet the O-RAN timing requirements for all configuration modes
- Benefits of using Renesas' ClockMatrix Family of synchronizers to guarantee both synchronization and low-noise sampling clocks for the RF converters and LO
- Benefits of using Renesas' PTP Clock Manager Software for Linux (PCM4L) with the ClockMatrix Family of synchronizers to guarantee IEEE 1588 compliance
- How the PMOD type 6A hardware architecture makes it simple to connect to any Renesas development kit
- How the integrated software reduces integration effort by providing software libraries and simple software APIs
- How the combined hardware and software solution of the Renesas Quick Connect system simplifies the transition from prototype to production
In this session, we will examine the implementation of Trustzone-M in Renesas Cortex-M33 based RA4 and RA6 MCUs, along with the additional features that build on top of this to further enhance embedded security. Also covered will be the software development tools that provide the necessary workflows to allow customers to deliver a secure system.
eProsima is the company behind micro-ROS and it is key-partnering with Renesas. The Renesas RA Family of microcontrollers is the micro-ROS recommended MCU and provides professional technical support at [email protected]. This webinar gives you the key insights of ROS and micro-ROS. We will demonstrate how to develop open source robotic applications using the RA Family.
During this webinar, we're going to:
- Highlight the key functionality of the DA16200 Ultra-Low Power Wi-Fi SoC
- Highlight and explain the extended AT Command functionality
- Show wi-fi implementation details on the RA6M4 MCU host
- Demonstrate ready-to-go ultra-low power wi-fi using Renesas RA6 Series MCUs as an example using the SparkFun Wi-Fi Shield
Renesas is contributing to the acceleration of customer development through our Winning Combination system solutions. The Webinar is focusing on two xEV applications, BMS*1 & inverter. For BMS, our application model & software solution reduces R&D*2 effort by providing sample application models that estimates SOC*3 & SOH*4. For xEV inverter, Renesas can help customers shorten development time by supporting system level functional safety.
*1 Battery Management System, *2 Research and Development, *3 State Of Charge, *4 State Of Health
Key takeaways
Jumpstart the process of learning the Renesas environment
Speed up time to market with sample models, reducing rework in BMS development
Reduce both application software and firmware development effort for BMS
Support for functional safety concept reduces development time at the system level for xEV inverter
Speakers:
Mr. Masuo Okuda, Senior Manager, Automotive Analog Marketing and Advanced Engineering Department, Automotive Analog Product Marketing Division, Renesas Electronics Inc.
Mr. Masashi Tsubota, Senior Principal Specialist, Automotive Analog Marketing and Advanced Engineering Department, Automotive Analog Product Marketing Division, Renesas Electronics Inc.