3D Printer
3D printers are attracting attention as the prices of personal hobby- use low-cost versions drop. Many low-cost 3D printers use the fFused dDeposition mModeling method and control 3D coordinates by controlling a plastic outputting head in 2D coordinates and controlling the height of the stage. A plastic loader motor and a cooling fan motor also require PWM output. In addition, large-capacity flash ROM and a high-performance CPU are required for high-speed processing of large volume data. Also required are serial I/O for receiving datae from a PC via USB or flash memory media devices and controlling LCD panel modules.
Renesas Electronics offers the RX200 Series, which has a high-performance CPU, PWM for controlling stepper motors, and serial I/O for communicating with various peripheral devices, and the RX600 Series, which has an RSPI for controlling serial flash.
System Control MCU
Semiconductor Device | Recommended Products | Features, etc. |
---|---|---|
System Control MCU | RX651 |
|
RX231 |
|
|
RX113 |
|
|
RL78/G1C |
|