SOTB™ 制程工艺
Energy Harvesting in Embedded Systems is Now a Reality
Exclusive SOTB technology from Renesas breaks the previous trade-off between getting either low active current or low standby current consumption – previously you could only choose one. With SOTB, you get both without compromise. Additionally, SOTB supports high operating frequency for high performance and small silicon node geometry for high-density memory. This is a recipe for very capable, extreme low-power applications that run from harvested ambient energy – no batteries required.
Extreme Low-Power Applications
什么是SOTB制程工艺?
A disruptive extreme low-power technology exclusively from Renesas.
SOTB的优势是什么?
Extreme low active and standby power, speed scalability, high performance analog with low noise, and high immunity to disruption from particle radiation.
RE Family Based on SOTB Process
The new product family using the SOTB™ process has been renamed the RE Family and the first product has been released.
First Product: RE01 Group
The RE01 Group is the first product of the RE Family.
electronica 2018 / Battery-less Velocity Measurement
(1min 14sec)
electronica 2018 / Battery-less ECG Heart Monitor
(1min 13sec)