概要

A battery control system is used for managing remaining battery capacity and control of battery charging and discharging. The voltages of the individual cells are monitored, and the balance controlled by the lithium-ion battery cell monitor ICs. The battery management MCU provided by Renesas can perform management of remaining battery capacity and battery charge control. In addition to the battery management MCU, Renesas supplies analog and power devices suitable for battery control systems.

系统框图

Battery Control System

Battery Control System Block Diagram

*BMIC: Battery Management IC

Automotive Development Tools Icon

开发工具

通过与众多工具供应商的合作,瑞萨电子为各种汽车系统提供开发工具。