下载 (D6003106)

发布日期 : Feb.26.19

类别 : Others

User's Manual for e-AI Translator V1.0.2



Description

The e-AI Translator is a tool that converts and imports the inference processing of neural network models which have been trained in an open-source deep-learning framework, Caffe or TensorFlow, into files of source code for the e² studio integrated development environment for MCUs and MPUs.
This document describes the methods of installation, usage, and points for caution of the e-AI Translator.

下载

产品名称 文档 名称 文档 大小 下载链接
User's Manual for e-AI Translator V1.0.2 r20ut4135ej0300-e-ai.pdf 1.13 MByte