Medium One, Inc.

类别: Cloud Connection , Development

Demonstrates that a heartbeat signal can be sent over Ethernet or Wi-Fi from a Synergy Kit to the Renesas IoT Sandbox web interface.

Details

This demo uses the Synergy SK-S7G2 Starter Kit and the AE-Wi-Fi application example kit to illustrate:

  • Data transfer to a cloud platform for analytics
  • Interactive LCD display of cloud analytics, built with GUIX™
  • Unified onboarding and provisioning for both Ethernet and Wi-Fi (GT202)
  • The Synergy SK-S7G2 kit first tries to connect to Ethernet then switches to Wi-Fi if Ethernet is unavailable.

Once connected the kit sends a heartbeat signal once per minute to the cloud. The Renesas IoT Sandbox web interface shows the heartbeat graphically or as a list of events. Cloud analytics such as duration and counter are displayed on the QVGA color LCD.

Copyright Disclaimer

© 2017 Medium One. All Rights Reserved.

 

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

/zh/products/synergy/gallery/partner-projects/medium-one-heartbeat/jcr:content/gallerydownload

Download

版本 1.0.0

当前版本

发布日期: 2017-06-23

支持的MCU: S7G2

MD5: c80a763e5ea3dff043732c9596cb1ef9

下载

最新消息

N/A

安装说明

Installation instructions are provided in the accompanying application note. 

/zh/products/synergy/gallery/partner-projects/medium-one-heartbeat
/zh/products/synergy/gallery/partner-projects/medium-one-heartbeat/jcr:content/allversionsection