Demonstrates Bluetooth® Classic connectivity to pair and transfer messages between devices using the Bluetooth Serial Port Profile (SPP).

Details

Uses the Bluetooth® SPP Pro app running on an Android smartphone to pair with nearby Bluetooth® devices. The Bluetooth® Serial Port Profile (SPP) of the ClarinoxBlue protocol stack with Bluetooth® Classic runs on the Renesas PE-HMI1 Kit to connect and transfer bidirectional data.

 

The ClarinoxBlue stack includes a built-in protocol analyzer for simplified debugging that allows custom application commands to be sent using the DLL-based plug-in interface. It offers threading, memory usage and memory leak analysis, along with an API for messaging between processors.

Copyright Disclaimer

Copyright 2017 Clarinox Technologies Pty Ltd. All Rights Reserved.

 

The content included herein has been provided by other companies and Renesas does not claim any ownership therein. Renesas may or may not moderate or pre-screen the content included herein. Renesas requires partners to verify the functionality of their products on Synergy Platform and Renesas is not responsible in any way for the content included herein nor its quality. Renesas does not endorse any content included herein or any opinion, recommendation, or advice expressed therein, and Renesas expressly disclaims any and all liability in connection with such content, whether or not arising under the laws of copyright, libel, privacy, obscenity, or otherwise. Renesas does not provide support for any of this content; all support requirements should be directed to the owner or licensor of the content. Renesas retains the right, at its sole discretion and without prior notice, to pre-screen, refuse, or remove any content from the Synergy Platform.

/zh/products/synergy/gallery/partner-projects/clarinox-bluetooth-spp/jcr:content/gallerydownload

Download

版本 1.0.0

当前版本

发布日期: 2017-06-23

支持的MCU: S7G2

MD5: 398e461548e172d8288676a537791c86

下载

最新消息

N/A

安装说明

This application has the following hardware requirements:

  • Renesas PE-HMI1 Synergy S7 kit
  • Smart Phone or mobile device

 

Installation instructions are included in the application project guide.

/zh/products/synergy/gallery/partner-projects/clarinox-bluetooth-spp
/zh/products/synergy/gallery/partner-projects/clarinox-bluetooth-spp/jcr:content/allversionsection