Renesas' radiation hardened comparators are fabricated using our dielectrically isolated radiation hardened silicon gate (RSG) process, which provides immunity to single event latch-up (SEL) and highly reliable performance in the space environment.

description文档

文档标题 language 类型 文档格式 文件大小 日期
应用指南 & 白皮书
AN9867: End of Life Derating: A Necessity or Overkill 应用文档 PDF 338 KB
其他
Intersil Space Products Brochure 手册 PDF 3.16 MB
Intersil Commercial Lab Services 手册 PDF 364 KB

print新闻及更多资源

类型 日期 降序排列
Rad Hard Test Reports 基本页面 2020年3月20日
Rad Hard SMD Test Flow 基本页面 2020年3月20日
Standard Data Package 基本页面 2020年3月20日
Low Dose Rate Acceptance Testing 基本页面 2020年3月26日