Capacitive Touch Evaluation System for RA2L1
The RA2L1 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the box...
QE for Capacitive Touch is a tool for assisting in the development of embedded systems that include the use of capacitive touch keys.
This tool simplifies the initial settings of the touch user interface and the tuning of the sensitivity.
Product Name | Latest Ver. | Released | Target Device (Note1) | Details of upgrade | Download | Operating Environment |
---|---|---|---|---|---|---|
QE for Capacitive Touch | V3.3.0 | Jun 20, 2023 | RA Family RL78 Family RX Family Renesas SynergyTM | See Release Note | Download | e² studio plug-in(Note2)(Note3) Operating Environment |
Notes
The RA2L1 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the box...
The RA6M2 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the box...
The RL78/G16 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the...
The RL78/G22 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the...
The RL78/G23 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the...
The RX130 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the box...
The RX140 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the box...
The RX671 capacitive touch evaluation system makes it easy for users to evaluate touch solutions offered by Renesas. You can start evaluating immediately out of the box...
QE for Capacitive Touch from Renesas enables the development of touch sensors by simply following a guide on a GUI, thus contributing to shortening the development period for touch sensor functions that take advantage of the performance of Capacitive Sensing Unit (CTSU2).
博客 | 2023年11月21日 | ||
博客 | 2022年5月17日 |
Simple GUI operations allow even a beginner to create the configuration for use with a touch user interface, monitor the state of input through the touch sensors, and adjust parameters.
Furthermore, since this tool can adjust tuning parameters and reflect the results through display in real-time, it is very useful for finding the appropriate parameters in various situations, such as in the presence of much static electricity or in cases of use with wet hands.
This tool enables automatic tuning for the sensitivity of the capacitive touch sensors. You can complete basic tuning within a few minutes by following the instructions in the pop-up messages.
You can develop a gesture application that reacts "by anyone's hand" without any specialized skills just by actually performing the gesture that you want AI to remember on the capacitance sensor.
e-AI × 3D Gesture Recognition >>
Usage Example of e-AI × 3D gesture recognition feature >>
Device | Driver | Version |
---|---|---|
RA Family | CSTU (Capacitive Touch Sensing Unit) Driver Flexible Software Package (FSP) Component for RA Family Component name: r_ctsu | V4.4.0 |
Touch Middleware Flexible Software Package (FSP) Component for RA Family Component name: rm_touch | V4.4.0 | |
RX Family | Driver for capacitive touch sensor unit RX Family QE CTSU Module Using Firmware Integration Technology Module name: r_ctsu_qe | V2.20 |
Middleware for touch sensors RX Family QE Touch Module Using Firmware Integration Technology Module name: rm_touch_qe | V2.20 | |
RL78 Family | Driver for capacitive touch sensor unit RL78 Family QE CTSU Module Software Integration System Module name: r_ctsu | V1.40 |
Middleware for touch sensors RL78 Family QE Touch Module Software Integration System Module name: rm_touch | V1.40 | |
Renesas Synergy | CTSU (Capacitive Touch Sensing Unit) Driver Synergy Software Package (SSP) Component for Renesas Synergy Component name: r_ctsuv2 | V2.2.0 |
Capacitive Touch Framework Synergy Software Package (SSP) Component for Renesas Synergy Component name: sf_touch_ctsuv2 | V2.2.0 |
See here for details on adding and setting middleware related to QE for Capacitive Touch