Information on the discontinuation of E1 emulator production and on its successor products

We have discontinued production of the E1 emulator due to components of the product having reached their EOL (end of life, i.e. end of production). Please click on the following link to confirm the details and our successor products.

[Notification] End of Life (EOL) Notice for E1 Emulator (PDF | English, 日本語)

 

Tool Chain Overview

 

图像
tool-v850

〈V850 Development Tool Lineup〉

MCU Real-time OS Software Tools On-chip debugging emulator Full-spec emulator Programmer
V850 RI850V4 (Note1)
RI850MP(V850E2M Dual Core)
Integrated Development Environment CS+ for V850
(includes integrated development environment (Note2), compiler, simulator, and emulator debugger)
E1 (Note4) IE850 PG-FP6 (Note5)
E1 (Note6)
Software Package for V850 [SP850]
(includes integrated development environment (Note3), compiler, simulator, and emulator debugger)
- -
  1. Some MCUs support the RX850V4 real-time OS instead.
  2. The integrated development environment is CS+.
  3. The integrated development environment is the project manager PM+.
  4. The E20 emulator may be used as well, but the supported debugging functions are equivalent to those of the E1.
  5. Used together with a programming GUI (FP6 Terminal).
  6. Used together with a programming GUI (Renesas Flash Programmer).

* CS+ is not generally promoted in the U.S. and Europe. For customers in the U.S. and Europe who are interested in CS+,
please contact our regional marketing departments for details.

* For details about which tools can be used with each MCU and specifications, see those user's manuals or release notes. The tools that can be used might differ depending on the MCU Part Name.