Renesas SmartConfig 4+

Renesas Electronics

Designed for iPad

    • Free

Screenshots

Description

The SmartConfig app from Renesas Electronics is a mobile application that works with devices which support the Renesas remote configuration service, such as Development Kits based on Renesas DA14531 Bluetooth® Low Energy SoC.

With the app you can connect to devices which support the configuration service and modify settings that are available on the peer device. Each device has its own extensible set of settings which are discovered by the app on connection.

What’s New

Version 3.520.4

- Rebranded app UI from Dialog Semiconductor to Renesas Electronics
- Bug fixes and improvements

App Privacy

The developer, Renesas Electronics, indicated that the app’s privacy practices may include handling of data as described below. For more information, see the developer’s privacy policy.

Data Not Collected

The developer does not collect any data from this app.

Privacy practices may vary, for example, based on the features you use or your age. Learn More

More By This Developer

GATTBrowser
Utilities
Renesas SUOTA
Utilities
Renesas SmartConsole
Utilities
Renesas SmartTags
Utilities
Renesas WiFiProvisioning
Utilities
Renesas SmartBond
Utilities

You Might Also Like

RenesasSST
Utilities
KSI BT Net
Utilities
Lora Gateway
Utilities
XTGateway
Utilities
XTPenetrate
Utilities
CheckBlue
Utilities