Target Board for RX23W
The Target Board for RX23W provides an entry point to evaluation, prototyping and developing for the RX23W MCU. Moreover, since this board incorporates an emulator...
低功耗 (LE) 蓝牙™是一种低能耗模式的蓝牙无线技术。低功耗蓝牙对电力消耗有所影响,特别是利用电池运行的应用场合。 低功耗蓝牙最具吸引力的一点,就是它可以在运行的同时与智能手机和平板电脑中的应用程序相连接。 适用于医疗保健及健身设备、家用电器以及RFID 电子标签的低功耗蓝牙解决方案不断增多。这类设备可以利用信标(Beacon)在不使用电线的情况下通过低能耗的信号即可连接至智能手机。
瑞萨电子提供“RX23W 解决方案”,内置蓝牙 5.0 LE 和物联网设备所必需的安全功能,以及触摸键、USB 和 CAN 等丰富的外围功能,在单个芯片上实现了设备系统控制和无线通信。 RX23W 支持诸如蓝牙5.0 LE的远程和网状网络之类的全部功能。通过支持“信道选择算法#2”,它更能抵抗来自其他2.4GHz RF信号的干扰,即使在存在无线电干扰的环境中也能实现稳定的通信。
This guide summarizes the Bluetooth LE MCU RX23W Solution and related resources for each product development phase. Please download and use it.
RX23W 集成了专用于蓝牙的高精度、低速、片上振荡器,无需外部匹配电路和外部电容器。
Renesas offers a lineup of module products that have built-in antennas and oscillators and have been certified by the Radio Law of each country. Despite being the world's smallest module size, many microcomputer peripheral function pins can be used.
These evaluation boards are best suited for the evaluation of Renesas' RX23W device/module, evaluation of Bluetooth LE functions and performance, and use for principle prototyping.
RX23W 目标板为 RX23W MCU 的评估、原型制作和开发提供一个切入点。 此外,由于此目标板集成了调试器,您可以将其用于自己的应用设计,而无需进一步投资开发工具。 这款产品提供通孔形式的引脚接头,可连接所有 MCU 的信号引脚,从而可以使用面包板轻松地进行原型设计。
RX23W 模块目标板为 RX23W 模块产品的评估、原型制作和开发提供一个切入点。 此外,由于此目标板集成了调试器,您可以将其用于自己的应用设计,而无需进一步投资开发工具。 这款产品提供通孔形式的引脚接头,可连接所有 MCU 的信号引脚,从而可以使用面包板轻松地进行原型设计。
The Renesas Solution Starter Kit for RX23W is the perfect starter kit for developers who are new to the RX23W (Code Flash 512KB, Pin Count 85-pin). The kit includes an LCD display module and an on-chip debugging emulator. Download the integrated development environment from the Renesas website and start evaluating RX23W performance, right after unboxing the Renesas Solution Starter Kit.
低功耗蓝牙协议栈是运行 RX23W 的必备软件,正在确认蓝牙 v5.0 规范。 支持 Core Specification v5.0 的所有 LE 功能。 而且根据功能集提供三种类型的库,以便选择适合最终产品规格的配置。
提供蓝牙认证 56 种类型(截至 2019 年 12 月)的标准配置文件/服务。
The profile is generated from QE for BLE[RA,RE,RX]. You can also design and generate a custom profile. Renesas also provides sample programs as a reference for your program development. The sample programs will be further expanded in the future.
Available sample programs:
示例程序 | 概述 |
---|---|
Beacon, Central, Peripheral, Multi-role Sample Program | Bluetooth Low Energy Application Developer's Guide and operates on the Target Board for RX23W. RX23W Group Bluetooth Low Energy Application Developer's Guide Rev.1.30 (ZIP | English, 日本語) |
Custom Profile Sample Program | This sample program provided as demo project "LED Switch Service" of "RX23W Group BLE Module Firmware Integration Technology Application Note - Sample Code". RX23W Group BLE Module Firmware Integration Technology Application Note Rev.2.50 - Sample Code (ZIP) |
RX23W Group Firmware update over the air sample program Rev.1.11 - Sample Code (ZIP | English, 日本語) | This sample program operates on the RX23W and realizes Over The Air (OTA) firmware update by Bluetooth LE wireless communication. |
RX23W Group Apple Notification Center Service Sample Program Application Note Rev.1.00 - Sample Code (ZIP) | The Apple Notification Center Service (ANCS) sample program operates on the Target Board for RX23W and connects to iOS devices using Bluetooth LE wireless communication. |
RX23W Group Sample Program for Highspeed Communication Rev.1.00 - Sample Code (ZIP) | This sample application sets the GAP parameters to optimal values and uses LE 2MPHY to realize high throughput Bluetooth LE wireless data communication between pairs of the Target Board for RX23W. Both central and peripheral side projects are provided. |
Bluetooth Mesh Stack:
The Mesh profile is provided as a dedicated library "Bluetooth Mesh Stack", so please use this to develop products that conform to the Bluetooth Mesh Networking specification. Bluetooth Mesh is a network optimized for building large-scale device networks, enabling multipoint-to-multipoint device communication. This technology is suitable for IoT solutions where performance, reliability, and security are important, such as building automation, sensor networks, and asset tracking.
Available sample programs:
示例程序 | 概述 |
---|---|
RX23W Group Temperature and Humidity Sensor Data Communication Sample Code Using Bluetooth Mesh Network Rev.1.01 - Sample Code (ZIP) | This is a sample program that communicates temperature and humidity sensor data using the Sensor Model included in the Bluetooth Mesh module. By using the Mesh network, it will be possible to transmit data over long range, easily expand the network, and build a network that is resistant to communication failures. |
我们提供了适应各种应用开发需求的蓝牙 LE 软件解决方案。 有关更多信息,请参阅协议栈产品页面。
QE for BLE[RA,RE,RX] 是一款专用工具,用于在支持低功耗蓝牙协议栈的系统中开发嵌入式软件。 此解决方案工具包在集成了e² studio 的开发环境中运行。e² studio 与 QE for BLE[RX] 相结合,可轻松测试瑞萨蓝牙 LE 微型计算机 RX23W 的通信功能,从而缩短产品上市时间。 使用此工具生成标准配置文件。 此外还可以设计并生成自定义配置文件。
有关更多信息,请参阅 QE for BLE[RA,RE,RX]: 低功耗蓝牙开发辅助工具页面。
TryBT 是一款智能手机示例应用程序,支持与蓝牙 LE 产品通信的功能。 您可以使用预装在 RX23W Target Board 中的固件来验证通信功能。对RA4W1 也同样有效。
另外,我们还提供对应的图标图像以及 Android Studio 项目与源代码,因此您可以在概念验证阶段将此应用程序示例用作开发蓝牙 LE 通信应用程序的基础。
TryBT 下载:
The Windows 10 Bluetooth LE application is an application example for Windows 10 that communicates with the firmware pre-installed on the evaluation board "Target Board for RX23W" or "Target Board for RX23W module", controls the LED blinking interval on the evaluation board and counts the number of times the switch is pressed.
In addition, a set of projects that can be launched and used in Visual Studio 2017 are provided, so you can use this application example as a base for developing Bluetooth LE communication apps that run on Windows in a Proof of Concept (PoC) phase.
Windows 10 Bluetooth LE 应用程序下载:Bluetooth LE microcomputer / module Windows 10 Bluetooth LE Application Rev.1.00 - Sample Code (ZIP) (PDF文档+Visual Studio 2017项目集)
在开发过程的“调查/评估”阶段,可以通过使用 BTTS(蓝牙测试工具套件)来评估由 RX23W 提供支持的 蓝牙 LE 的功能和性能,了解新的 LE 功能、API 执行过程和 API 参数。
在设备的“认证”阶段,它可以用作 GUI 工具,用于在 Radio Law 认证测试中操作被测设备 (DUT)。
BTTS 下载:Bluetooth LE MCU Bluetooth Test Tool Suite operating instructions Rev.1.07 (ZIP | English, 日本語) (PDF 文档 + Windows 应用程序)
RX23W 的目标应用:
瑞萨还提供了许多引人注目的模拟+电源+嵌入式处理+ 连接的"成功产品组合"。
解决方案标题 | 概述 |
---|---|
医疗保健 | |
呼吸机系统 | 这是一个呼吸机系统参考设计,可以提供在走廊或非 ICU 病房使用的便携式呼吸机。 面罩上连接了一个近端空气压力传感器,可以监测吸气压力,并将这一信息发送给 RX23W MCU。 |
医疗贴片 | 这款安全、可重复使用的便携式健康监测设备,可实现医疗保健互联,通过安全的 Bluetooth Low Energy 连接进行体温、血氧饱和度 (SpO2) 和心率监测。 该医疗贴片采用可充电锂离子电池,打造精致的外形,并增强了可重复使用性。 |
Electronic Drug Delivery System | A solution for healthcare drug delivery devices such as infusion pumps or insulin pumps. This design uses a combination of two MCUs, which includes the latest RA6M3 for motor control and sensor measurement, and the RX23W for Bluetooth Low Energy wireless communication. It also includes analog components, like DC/DC regulators, an Li-ion battery charger, a MOSFET bridge driver, and a factory-calibrated flow sensor. |
家庭 / 楼宇自动化 | |
适用于家居自动化或楼宇 HVAC 系统的室内传感器 | The indoor/outdoor sensor unit(s) for automatic home or building HVAC systems provide measurements via Bluetooth Mesh to a master actuator. |
适用于家居自动化或楼宇 HVAC 系统的室外传感器 | |
适用于家居自动化或楼宇 HVAC 系统的主执行器 | |
适用于家居自动化或楼宇 HVAC 系统的从执行器 | |
气象监测站解决方案 | 该解决方案支持智能家居系统,其中主控单元(室内单元)汇聚从单元(室外单元)测量的天气数据(温度、湿度、CO2 浓度)。 |
适用于家居自动化或楼宇 HVAC 系统的 IP 网关 | IP 网关是一种到内部网/互联网的可选网桥,用于传感器和/或控制数据。HTTPS 或 MQTT (以及其他选项)可用于安全协议需求。 |
Contact Information:
E-mail: [email protected]
Tel: +1-657-218-5199
https://www.silextechnology.com/
The available SX-23BT microcomputer module is compatible with Bluetooth 5.0 LE and includes an RX23W MCU.
The SX-23BT is microcontroller module supporting Bluetooth 5.0 Low Energy for IoT endpoint devices with the following features.
By connecting the Renesas E2 emulator, immediate evaluation is possible. In addition to the FINE interface connector, it also has through holes for pin headers that enable access to MCU signal pins. You can easily prototype IoT devices by attaching sensors and other parts to this evaluation board.
Please refer to the Knowledge Base for FAQs on Bluetooth specifications, MCUs, modules, protocol stacks, development environments, qualification, and more.
Software title
|
Software type
|
公司
|
---|---|---|
Bluetooth® Low Energy Protocol Stack for RX family Bluetooth v5.0 certified protocol stack [Target device: RX23W]
|
Protocol Stack | 瑞萨电子 |
QE for BLE: Development Assistance Tool for Bluetooth® Low Energy Debugging support tool that specializes in Bluetooth® Low Energy system development [Plugin for Renesas IDE "e² studio"] [Support MCU/MPU: RA, RX, RL78]
|
Solution Toolkit | 瑞萨电子 |
e² studio 基于 Eclipse 的瑞萨集成开发环境 (IDE)。
[支持MCU/MPU:RA、RE、RX、RL78、RH850、Renesas Synergy、RZ]
|
IDE and Coding Tool | 瑞萨电子 |
Renesas Flash Programmer (Programming GUI) Flash memory programming software [Support MCU/MPU and devices: RA, RE, RX, RL78, RH850, RISC-V MCU Renesas Synergy, Power Management, Renesas USB Power Delivery Family, ICs for Motor Driver/Actuator Driver, V850, 78KR, 78K0]
|
Programmer (Unit/SW) | 瑞萨电子 |
4 items
|
博客 | 2021年9月2日 | ||
博客 | 2021年9月2日 | ||
博客 | 2021年3月31日 | ||
博客 | 2020年6月13日 |