RapidIO’s Unique Blend of Ultra-Low Latency and Scalability Help Ensure Excellent User Experiences for Video Applications  

2016年4月27日

SAN JOSE, Calif., April 27, 2016 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today that electronics giant Huawei has selected IDT’s RapidIO technology to help deliver superior video quality for its new video platform. Huawei chose IDT® RapidIO® for its potent blend of ultra-low latency and scalability, which enable top-shelf high-definition video solutions.

The company has integrated IDT’s RapidIO technology for video processing in multiple generations of products. IDT RapidIO technology is ideal for the data-intensive video system tasks of encoding, decoding, caching, streaming and analytics. Huawei achieved the video performance it needed for its new processing-intensive platform by using multi-core CPUs in a RapidIO-switched network through IDT’s PCIe-to-RapidIO interconnect silicon.

“Applying IDT’s RapidIO interconnect switching and network interface silicon are key elements of ensuring a high-quality high-resolution end user experience in our next-generation video systems,” said Xu Fugang, project manager for Huawei’s videoconferencing product line. “We have been using IDT RapidIO products in multiple generations of our product line for their low latency, scalability and overall energy efficiency that is best in class when trying to connect a large number of processors in a system to do real-time image processing and associated computing.”

IDT’s RapidIO interconnect, high-performance timing and memory interface products are optimized for a variety of video system solutions. These include video conferencing, broadcast video, video caching and distribution, and video edge analytics, where a combination of low latency, high throughput and optimized system timing are critical to delivering a state-of-the-art solution.

“Our RapidIO products have been designed into multiple applications around the world where low latency and scalability are prerequisites,” said Sean Fan, vice president and general manager of IDT’s Interface and Connectivity Division. “Huawei’s new video system is one of many examples of IDT’s success in enabling the video-centric internet and 5G networks.”

IDT has shipped more than 110 million ports of RapidIO for use in production systems. IDT recently announced its next-generation RXS RapidIO switch family, of even faster 50 Gbps port speeds that can support 600 Gbps of switching in a single switch or 4.8 Tbps at rack scale.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers' applications. IDT's market-leading products in RF, timing, wireless power transfer, serial switching, interfaces and sensing solutions are among the company's broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol "IDTI." Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. RapidIO is a registered trademark of RapidIO, Inc., doing business as the RapidIO Trade Association. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.