IC Combines Remaining Battery Capacity Detection and Charging Functionality on a Single Chip, Enabling Charging Control Tailored to the Battery Characteristics

2015年7月23日

TOKYO, Japan, July 23, 2015 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced its new lithium-ion (Li-ion) battery fuel gauge IC, the RAJ240500, designed to extend battery life for connected mobile devices such as tablets, notebook PCs and smartphones. Leveraging its extensive design expertise in fuel gauge and charging ICs for mobile devices, Renesas has developed a single-chip device that delivers high-precision battery charge measurement and control that reduces the burden on the battery and contributes to longer device battery life. In addition, in order to facilitate the development using this product, Renesas is offering sample codes and evaluation tools as solutions, including the reference card circuit diagram.

Battery life has become an important decision factor for consumers purchasing mobile devices such as tablets and notebook PCs, creating strong demand for efficient battery charging and control technologies. In the past, battery control circuits had to treat the battery as being at ‘zero charge’ even when there was still some capacity remaining, and as ‘fully charged’ even when charging was not yet complete, in order to assure the safety of the battery. The resulting design challenge was a shorter battery life relative to charge capacity.

Battery degradation is another challenge. Li-ion batteries suffer from reduced capacity after repeated charge-discharge cycles due to deterioration of the materials they are made from. Repeated control when not fully charged or fully discharged reduces the number of charge-discharge cycles over the service life of the battery, which for many devices is equivalent to the service life of the device. To extend the usable battery duration and enable longer battery life while accounting for typical wear-and-tear changes, designers require charge control that decreases the burden placed on the battery and that reduces degradation as far as possible.

About the RAJ240500 fuel gauge IC:

The new Renesas fuel gauge IC addresses these design challenges with a two-in-one solution that combines advanced algorithmic fuel gauge IC functionality with charger IC functionality in a single device. Integrating battery charge measurement, or fuel gauge, and charging functionality on a single chip allows designers to achieve high-precision charging control that closely matches the battery status. This enables them to utilize the battery's capacity to the fullest extent to maximize the battery life per charge as well as reduce the battery load and degradation rate to extend service life.

Additional feature highlights include:

  • Single-chip integration for smaller form factors and reduced total system costs, including a high-efficiency power supply architecture system, the NVDC system (Narrow VDC) (Note 1), designed for tablet PC and notebook PC applications, which can reduce the number of components by approximately 20 percent compared to previous systems, as well as reduce the number of design man-hours required.
  • Rapid battery protection and response to assure a high level of system safety in abnormal battery conditions
  • On-chip flash memory that enables flexible settings and charging specifications, allowing easy accommodation of new product models.
  • Support for Dynamic Battery Power Technology, an advanced system control technology, to maximize the system performance according to the remaining battery amount (Note 2).

Pricing and Availability

Samples of the RAJ240500 are now available, priced at US$10 per unit. Mass production of the RAJ240500 is scheduled to begin in October 2015 and is expected to reach a volume of 10,000,000 units per month in October 2016. (Pricing and availability are subject to change without notice.)

Refer to the separate sheet (PDF: 57 KB) for the main specifications of the RAJ240500.

For more product information, please visit: https://www.renesas.com/en/products/power-management/battery-management-systems.html

(Note 1) NVDC (Narrow VDC) is a high-efficiency power architecture provided by Intel Corporation ®. By limiting the input voltage range of the system load, it aims to improve the power efficiency of the system.

(Note 2) Dynamic Battery Power Technology (DBPT) is an advanced system operation technology provided by Intel Corporation® and utilizes battery condition information to maximize system performance. To maximize the system performance, this technology leverages information such as the remaining battery capacity and the battery's characteristics.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.

(Remarks) All registered trademarks or trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.