Expanded RX100 Series Strengthens Line-Up for Cost-Sensitive Mobile Healthcare, Sensors, Building and Industrial Automation, and Smart Appliance Applications

2013年10月10日

TOKYO, Japan, October 10, 2013 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, has expanded its popular 32-bit RX100 Series of microcontrollers (MCUs) with the RX110 Group. Designed to support a broad range of markets, the new MCUs deliver a combination of ultra low-power consumption and high performance at attractive price points for entry-level 32-bit embedded Internet of Things (IoT) applications, including mobile healthcare, environmental sensors/detectors, smart appliances, and industrial and building automation. A complement to the RX111 Group announced in April 2013, the new RX110 MCUs combine RX core performance along with Renesas' True Low Power™ features, providing greater device scalability for these cost-sensitive applications.

Based on Renesas' RX CPU core, the RX100 Series of MCUs delivers high performance, ultra-low power, connectivity and digital signal processing (DSP) functionality in a general-purpose MCU. The new RX110 devices offer the industry's best active power/power-down mode capabilities, system performance and DSP implementation levels for entry-level 32-bit MCUs.

With best-in-class run-mode power consumption—as low as 100µa/MHz, 4.8µs wake-up time, and three low-power modes, including the lowest power-down mode with Real Time Clock (RTC), the RX110 MCUs enable extended life cycles for battery-powered applications such as blood glucose meters, remote control systems or POS terminals.

The new MCUs also feature three operating speeds, achieving 1.56 Dhrystone MIPS (DMIPS)/MHz throughput and 3.08 CoreMark®/MHz. In addition, with the RX110 Group, Renesas offers the only entry-level 32-bit line to provide a complete DSP library, as well as single-cycle Multiple/Accumulate and hardware-based Divide capability. This provides much-needed support for customers working in audio processing and digital filtering, as well as sensor-based applications.

To address critical compliance regulations, such as FDA/FCC certification and IEC60730 for enhanced safety, the RX100 Series—including the RX110 Group—features several safety and security functions and peripherals not available on any other entry-level 32-bit MCU, including:

  • On-chip clock frequency accuracy measurement circuit (CAC), which ensures the accuracy of the MCU's clock frequency
  • Data Operation Circuit (DOC), which allows for hardware-based RAM memory testing that is used to identify a potential memory fault
  • Cyclic redundancy check (CRC)—a hardware-based feature that prevents timing or corruption issues with the communication functions

As part of the RX100 Series, the new RX110 Group of MCUs joins the RX111 Group announced in April 2013, extending the RX Family line-up to support applications with ultra-low power, on-chip connectivity and cost-sensitivity constraints. The RX111 Group was the first member of the Renesas RX family to introduce True Low Power™ with 32-bit RX performance. The RX110 Group is easily scalable to the mid- and high-end RX600 and RX200 Series, providing greater flexibility and an easy migration path to higher integration levels and higher performance MCUs. This enables embedded designers to move easily between full-feature and cost-sensitive platforms with minimal re-design efforts and commitment.

Just like the RX111 Group, the new RX110 devices are supported by Renesas' extensive development tools ecosystem. This includes the Renesas Eclipse-based e² studio IDE and the Renesas RX compiler, IAR Systems' Embedded Workbench, as well as the RTOS kernels by Micrium, Segger, CMX, Express Logic, RoweBots, and FreeRTOS. The recently launched RX111 Promotion Board (RPB) provides a unique and cost-effective evaluation platform designed to facilitate the evaluation of Renesas' RX100 MCUs.

With the addition of the RX110 group of MCUs, the Renesas RX Family offers embedded designers one of the most comprehensive 32-bit line-ups that supports a broad range of applications, from the smallest, battery-powered equipment in which cost is the most important factor to the highest performance applications that require extensive data processing and computation.

Refer to the separate sheet for the main specifications of the RX110 Group of MCUs.

Pricing and Availability

Samples of the RX110 devices are available now, with mass production scheduled for March 2014 and expected to reach a scale of 1,000,000 units per month in December 2015. Pricing ranges from US$0.95 for an 8KB, 36-pin configuration in 10,000-unit quantities to US$1.51 for a 128KB flash, 64-pin configuration in 10,000-unit quantities. (Pricing and availability are subject to change without notice.)

(Remarks)
CoreMark® is a registered trademark of EEMBC®. EEMBC® is a registered trademark of the Embedded Microprocessor Benchmark Consortium. All other registered trademarks or trademarks are the property of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.