RX210 Group: the Industry’s Widest Range of Extremely Low Power 32-bit RX Devices Achieving as Little as 150 µA / MHz Current Consumption

2013年2月18日

Dusseldorf, February 18, 2013 – Renesas Electronics Europe, a premier supplier of advanced semiconductor solutions, today announced the availability of a large number of new low power, low voltage microcontrollers (MCUs). Renesas is expanding the low power, low voltage RX200 series to include versions offering from 64 KB to 1 MB of on-chip flash memory, and package sizes from 48-pin LQFP to 145-pin LGA. Combined with active mode power consumption of 7.2 mA at 50 MHz operation and a standby mode of 0.4 µA, this provides an industry leading 32-bit low power lineup.

The RX200 Series

The RX200 series of MCU is part of the RX family of 32-bit MCUs from Renesas. The powerful RX CPU core supports a wide range of applications, offering a huge range of solutions aimed at many applications such as metering, motor control and networking.
The RX200 series is based on an advanced, low power flash process, designed to meet the latest requirements of the next generation of lower power applications. The combination of the high performance 32-bit RX CPU, which delivers 3.08 CoreMark / MHz, and operation at voltages as low as 1.62 V and as high as 5.5 V, means that this RX200 series provides an ideal solution. The flash memory offers reprogramming across the full voltage range, from 1.62 – 5.5 V with E2data Flash 100k write erase cycles and guaranteed data retention of up to 30 years.

New RX210 group roadmap

The RX210 group now offers a unique lineup of low power, 32-bit devices, offering a wide range of memory size and package options and suitable to support every low power application that now needs 32-bit performance. The RX210 group supports many powerful on-chip peripherals, with a multitude of on-chip timers, including motor control timers, a Real Timer Clock and watchdog timers. The RX210 also includes up to 15 on-chip serial interfaces, including SPI & I2C support, a 12-bit ADC and 10-bit DAC, DMA controllers, an on-chip event system, a peripheral mapping controller and a wide variety of on-chip safety and reliability functions designed to support IEC60730 (VDE compliant software libraries available).
The combination of the high performance RX CPU with a wide range of operating voltage choices, flash sizes and available package options, makes the RX210 an ideal solution for a wide variety of applications, such as consumer products, data loggers, meters, small appliances and industrial sensors.

Availability

All the versions of the RX210 group are now available in sample quantities and will be available in mass production by the end of March 2013.

(Remarks)
All product names and service names that appear in this press release are all trademarks or registered trademarks of their respective owners.

About Renesas Electronics Europe

Renesas delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live – securely and safely. As the number one global supplier of microcontrollers, and a leader in A&P and SoC products, Renesas provides the expertise, quality, and comprehensive solutions for a broad range of Automotive, Industrial, Home Electronics (HE), Office Automation (OA) and Information Communication Technology (ICT) applications to help shape a limitless future.

Renesas Electronics Corporation was established in 2010 and is headquartered in Japan.With over 800 hardware and software alliance partners worldwide, it has the industry’s largest local support network. Renesas Electronics’ European structure is comprised of three business units – the Automotive, the Broad-based and the Industrial Solution Business Unit.

Further information about Renesas Electronics Europe is available at www.renesas.com

Renesas Electronics Europe is also on social media at http://twitter.com/Renesas_Europe, http://facebook.com/RenesasEurope and http://youtube.com/RenesasPresents.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.