IDT’s High-performance, Compact, and Flexible Universal Frequency Translator (UFT™) Timing Solution Captures Prestigious ACE Award Presented by UBM Tech’s EE Times and EDN
SAN JOSE, Calif., April 2, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it received a 2014 Annual Creativity in Electronics (ACE) Award in the ‘Ultimate Products’ category for the 8T49N28x Universal Frequency Translator (UFT) clocking family. The award was presented by UBM Tech’s EE Times and EDN, two prestigious industry publications.
“We are excited to receive a 2014 ACE Award for our industry-leading UFT timing solutions,” said Greg Waters, president and CEO at IDT. “As the leader in silicon timing, we provide a clear competitive advantage to our customers with our technical innovation and support tools. Offering eight programmable outputs and RMS phase jitter of less than 300 femtoseconds (fs), IDT’s UFT family is a powerful and flexible solution enabling the rapid deployment of complex, high-performance clock trees.”
IDT’s 8T49N28x UFT family is the industry’s first single-chip programmable solution capable of generating eight different output frequencies with less than 300 fs RMS phase jitter over the standard 12kHz to 20MHz integration range. The devices offer independently-programmable clocking outputs with the flexibility to apply virtually any input frequency and select virtually any output frequency. The high level of integration and low jitter eliminates the need for separate jitter attenuation, frequency translation, and redundancy management – empowering engineers to save cost and board area through consolidation. These devices are ideal for high-performance optical networks, wireless base stations and 100 Gigabit Ethernet (GbE) interface applications.
Fully supported by IDT’s Timing Commander™ GUI (graphical user interface), the 8T49N28x family can be easily programmed to meet the system’s requirements without sifting through register tables in the datasheet. Additional GUI-based controls, calculations, and status monitors allow the user to experiment with and fine-tune the configuration. IDT’s Timing Commander software and 8T49N28x product configuration files can be downloaded online at www.idt.com/go/TimingCommander.
Product Availability
The IDT 8T49N281i, 8T49N282i, 8T49N283i are production-released and shipping in volume today. The 8T49N281i and 8T49N283i are available in a 56-lead 8 x 8 mm VFQFPN package, and the 8T49N282i is available in a 72-lead 10 x 10 mm VFQFPN package. For more information about IDT’s industry-leading portfolio of clocks and timing solutions, visit www.idt.com/go/timing.
About IDT Clock and Timing Solutions
With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. IDT has also expanded its portfolio to include frequency control products, such as the XpressO® oscillators from Fox Electronics and an innovative line of MEMS oscillators that are rapidly replacing legacy quartz-based oscillators. For more information about IDT’s leading portfolio of timing products, please visit www.idt.com/go/timing.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.