IDT RapidIO Switch Enables RADVISION to Meet High-Performance, Low-Latency and Multicast Support Requirements

2011年3月8日

SAN JOSE, Calif., March 8, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that the IDT Tsi578 RapidIO switch has been selected by RADVISION Ltd., a leading provider of unified video communications solutions, for use in its SCOPIA Elite multipoint video conference system. RADVISION selected IDT’s RapidIO switch product because of its high performance, low latency, and robust feature set which enables them to deliver uncompromised high-definition multipoint continuous presence.

          Today’s high-performance video and imaging systems require higher resolution and more frames per second for the best user experience. Existing semiconductors, such as DSPs and FPGAs support the processing, but demand a specialized digital “pipe” to transfer large amounts of data in real-time. RapidIO is an ideal solution, providing cost and performance benefits that facilitate the broad deployment of premium video systems across various industries.

          The IDT Tsi578 is a third generation RapidIO switch used as a chip-to-chip, board-to-board, and chassis-to-chassis interconnect supporting up to 80 Gigabits per second of full duplex aggregate bandwidth. Using RapidIO, OEMs in imaging, video, server, defense, wireless and industrial markets are able to design embedded systems with peer-to-peer clusters of embedded processors with reliable packet transmission, simplified system memory maps, and ultra-low end-to-end packet termination latency with three layers of protocol terminated in hardware.

          “After extensive embedded technology analysis, we chose IDT’s RapidIO switches because of the ease of designing a multi-DSP system in a peer-to-peer network with low and deterministic latency, ample bandwidth, low power, and excellent software scalability; all of which were critical to our SCOPIA Elite video conference system,” said Orly Nicklass, vice president of research and development at RADVISION. “RapidIO helped simplify our system design due to its friendly protocol attributes. These features, coupled with IDT’s powerful software and system modeling support allowed us to design a distinguished product and gain a competitive advantage.”

          “We’re pleased that RADVISION has selected IDT’s RapidIO switch for its video conferencing system,” said Fred Zust, vice president of the Communications Division at IDT. “The merits of RapidIO make it ideal for high-performance video, enabling wide spread deployment of these video systems with low cost and power.  We’re delighted to have contributed to RADVISION’s superior product, and look forward to continuing to support them in the future.”

          The IDT Tsi578 is one of a series of RapidIO switch offerings from IDT, including Gen 2 RapidIO devices.  IDT’s rich portfolio provides a wide selection of port and lane count devices that allow customers to tailor their switch selection to the application. For more information about IDT’s RapidIO solutions, visit www.idt.com/go/S-RIO.

About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, combines analog and digital technology to develop system-level innovations that optimize customers’ applications and enrich the end-user experience. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

About RADVISION
RADVISION (Nasdaq: RVSN) is the industry’s leading provider of market-proven products and technologies for unified Visual Communications over IP, 3G and IMS networks. With its complete set of standards-based video communications solutions and developer toolkits, RADVISION is driving the Unified Communications evolution by combining the power of video, voice, data and wireless – for high definition Video Conferencing Systems, innovative converged mobile services, and highly scalable video-enabled desktop platforms on IP, 3G and emerging next-generation IMS networks. To gain additional insights into their products, technology and opinions, visit blog.radvision.com. For more information about RADVISION, visit www.radvision.com.

 ###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.