Full compliance testing ensures customers can confidently design ITU-T G.8262-compliant Synchronous Ethernet equipment with joint solution comprised of IDT’s Synchronous Timing components and Marvell’s 10G Ethernet devices.

2018年4月26日

SAN JOSE, Calif., April 26, 2018 – Integrated Device Technology, Inc. (IDT) (NASDAQ: IDTI) introduced today a Synchronous Ethernet solution for 4G/5G mobile networks using Marvell’s Alaska X family of devices. Synchronous Ethernet (SyncE) provides the ability for frequency distribution and synchronization over Ethernet-based packet networks. SyncE helps service providers meet the challenges of increasing bandwidth, coverage and mobile application layer services which require high-accuracy synchronization. In addition, SyncE improves the reliability of time synchronization of 4G/5G base stations working in conjunction with IEEE 1588.

The joint solution has been pre-tested to pass all ITU-T G.8262 compliance testing including wander transfer, tolerance and generation. The solution, which features the Marvell® 88X3340P Alaska X 10Gigabit Ethernet PHY and IDT® 82P33831 synchronization management unit, allows end-customers to design products compliant to the ITU-T G.8262 specification if the proven recommendations are followed.

The two companies have also released a white paper titled SyncE Wander Testing for Marvell 88X3340P and IDT 82P33731 that highlights challenges solved by the joint solution to achieve standards compliance and includes relevant testing data and design specifications, to aid customers. The simple, proven reference design solutions in the paper are presented using the IDT and Marvell devices. This white paper details the first of several planned pre-tested solutions to demonstrate system performance and provide technical guidance to simplify customers’ design efforts. 

“Ensuring a system is compliant to ITU-T standards can be a major concern, but IDT and Marvell have taken that concern away,” said Kris Rausch, vice president and general manager of IDT’s Timing Products Division. “By using this proven solution with readily-available silicon from our two companies, customers can focus on other areas that bring value to their products without worrying about G.8262 compliance.”

            “IDT’s synchronization management unit pairs up nicely with Marvell’s industry-leading 10 Gigabit Ethernet PHYs,” said Chris Koopmans, executive vice president, Networking & Connectivity at Marvell. “By taking advantage of our PHYs’ SyncE support, the combined system allows customers to build high-performance Ethernet solutions that support the high-accuracy time synchronization required by today’s demanding 4G/5G application layer services.”

Visit idt.com/marvell to download the white paper and get more details on the reference design solution. For more information about IDT's industry-leading portfolio of timing solutions, visit idt.com/timing or contact your local IDT sales representative.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT’s market-leading products in RF, high performance timing, memory interface, real-time interconnect, optical interconnect, wireless power, and smart sensors are among the company’s broad array of complete mixed-signal solutions for the communications, computing, consumer, automotive and industrial segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT can be found at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

© 2018, Integrated Device Technology, Inc. IDT  and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc., and its worldwide subsidiaries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners

この記事をシェアする