IDT and Intel® Advancing Wireless Charging on Low-Power Solutions

September 9, 2014

SAN JOSE, Calif., Sept. 9, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) announced today at the Intel Developer Forum that it is working closely with Intel on the development of wireless charging solutions to accelerate the delivery and adoption of the nascent technology. As silicon and solutions leaders in wireless charging, the two companies  expect to bring a new generation of wireless capabilities that make charging consumer products easier than ever. Based on magnetic resonance technology, these capabilities will enable the charging of multiple devices simultaneously and through chargers built into objects such as tabletops. This collaboration is the latest step in IDT’s drive to deliver relief from the worry of running out of power, the clutter of wires, and the need to travel with chargers.

The two companies, both board members of the Alliance for Wireless Power (A4WP), will define, design and manufacture next-generation solutions that comply with the A4WP magnetic resonance standard. The new technology will offer the ability to charge both lower and higher power devices, from wearables and phones to tablets and PCs. The companies expect to have their technology in products in 2015.

"Intel's ‘No Wires’ vision will free consumers of dealing with power cables and deliver the easiest, most convenient way to charge all their devices, at home, at work and on the go,” said Sanjay Vora, vice president and GM of User Experiences for Intel. “We are excited to have IDT partner with us on bringing A4WP-based wireless charging to the market quickly and successfully."

“Intel and IDT together will deliver a new level of wireless charging capabilities to an increasingly un-wired world,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “Working closely together, we are fundamentally changing the way people power up their devices.”

About IDT Wireless Power

IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, YouTube and Google+.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. Intel (NASDAQ:INTC) is a registered trademark of Intel Corporation in the United States and other countries. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.