RA2A2 MCU产品组评估套件
EK-RA2A2 评估套件使用户能够轻松评估 RA2A2 MCU产品组的功能,并使用瑞萨电子的 灵活软件包 (FSP) 和 e2 studio IDE 开发嵌入式系统应用。 用户可利用丰富的板载功能,以及选择热门生态系统插件来将丰富创意变为现实。
入门
运行快速入门示例项目
- EK-RA2A2 开发板预编程了快速入门示例项目(EK-RA2A2...
QE for AFE V2.2.0 Release Note (PDF | English, 日本語)
- Support the new device RA Family RA2A2 group
- A [AFE Overview (QE)] view is newly supported in the stand-alone version
- Improve workflow when working in e² studio
QE for AFE is a development assistance tool that supports the development of embedded systems that handle high-precision sensing by using MCUs that include an analog front end (AFE).
Product Name | Latest Ver. | Released | Target Device | Details | Download | Operating Environment |
---|---|---|---|---|---|---|
QE for AFE | V2.2.0 | Mar 14, 2024 | RA Family RX Family | See Release Note | Download | Operating Environment |
Note: For detailed support devices, refer to "Target Devices".
EK-RA2A2 评估套件使用户能够轻松评估 RA2A2 MCU产品组的功能,并使用瑞萨电子的 灵活软件包 (FSP) 和 e2 studio IDE 开发嵌入式系统应用。 用户可利用丰富的板载功能,以及选择热门生态系统插件来将丰富创意变为现实。
瑞萨电子 RX23E-B 解决方案入门套件是一款评估工具,专为使用 RX23E-B 32 位微控制器 (MCU) 进行传感器测量而设计。 该套件包括一个 RX23E-B MCU 评估板,配备了用于传感器测量的外设和软件(可在网站下载)。 购买套件后,即可立即开始模拟特性的测定。...
EK-RA2A1 评估套件可通过瑞萨电子的灵活配置软件包 (FSP) 和各种 IDE,帮助用户对 RA2A1 MCU 群组的特性轻松进行评估,并对嵌入系统应用程序进行开发。
QE for AFE Tutorial: How to Import and Export AFE Adjustment Results
This video demonstrates how to import and export AFE adjustment results.
QE for AFE:https://www.renesas.com/qe-afe
This video describes the procedure for writing the AFE adjustment program and connecting to the PC.
QE for AFE connects with an EK-RA2A1 board via USB serial communication to configure AFE registers on the RA2A1 MCU, check the operations, and display the A/D conversion results.
The AFE-related registers including connection with analog IPs and PGA gain settings can be configured with a graphical user interface. Through serial communication with the evaluation board via USB, you can check connection with the evaluation board, acquire and configure register values, start an A/D conversion, and acquire the A/D conversion value (A/D conversion is performed in serial scan mode).
You can display a waveform and histogram and perform analysis for the acquired A/D conversion result.
Displays the frequency-gain characteristics curve for the SINC3 filter based on register configuration values.