概览

Vibration Harvester Unit (EH12) can generate power from slight vibration like walking motion. If the Bluetooth® Low Energy (LE) communication board is connected to EH12, the board can transmit a Bluetooth LE signal with the generated power. EH12 uses the Electro-magnetic method.

  • Power is generated by moving the magnet with respect to the coil
  • Highly efficient power generation by reducing leakage flux
  • Highly durable and highly reliable
  • Wearable Devices
  • IoT Products
  • Small Gadgets

文档

 

支持

资源

TOYONICS 外部链接