概览

The Battery-less Smart Farming Sensor solution uses Renesas RE Family’s energy harvesting functionality to create an ultra-low power, highly energy efficient, maintenance-free farming solution. The system is capable of measuring soil parameters like humidity, temperature, soil moisture, electrical conductivity, etc., and sending this information via Sub-GHz technology (LoRa®) to cloud for prediction and analysis.

  • The RE01 MCU will be in software-standby (or off) mode most of the time.
  • During its low-power mode, the Energy Harvesting Capability charges the rechargeable battery, checking its voltage level periodically.
  • When there is enough power stored, the MCU wakes and communicates with the temperature, humidity, electrical conductivity and soil moisture sensors and gathers the data.
  • The sensor readings are then sent out via LoRa (low-power wide-area) wireless communication.
  • A dashboard on a local PC/cloud displays the received sensor readings to the end-user.
  • Smart Agriculture Sector
  • Remote Sensing

文档

 

支持