图像
Yasuto Mochizuki
Principal Specialist
已发布: 2021年5月14日

Do you know the following?

The RL78/G14 Fast Prototyping Board and Wi-Fi-Pmod-Expansion-Board got AWS device qualification of FreeRTOS and it will be the first RL78 16-bit microcontroller (MCU) to be listed in the AWS Partner Device Catalog.

RL78 G14 Fast Prototyping Board | AWS Qualified (amazonaws.com)

As a result, the 16-bit MCU "RL78/G14", which contributes to the realization of the lowest power and low cost system among Renesas Electronics MCUs, can be connected to AWS by using FreeRTOS. And with a low-end MCU like the RL78, you can safely and easily connect IoT endpoint devices to the cloud.

In addition, the RL78/G14 Fast Prototyping Board and Wi-Fi-Pmod-Expansion-Board are sold at affordable prices. We have also prepared application notes such as "RL78/G14 Group Visualization of Sensor Information on Amazon Web Services using RL78/G14 Fast Prototyping Board and FreeRTOS", so you can feel free to try connecting to AWS.

RL78/G14 Fast Prototyping Board and various Application Notes.
RTK5RLG140C00000BJ - RL78/G14 Fast Prototyping Board

Wi-Fi-Pmod-Expansion-Board
Wi-Fi-Pmod-Expansion-Board - 802.11b/g/n 2.4G Wi-Fi Pmod Expansion Board
 

Figure. The system configuration from sensor information acquisition to visualization using this kit.

图像
RL78G/14 FPB AWS Cloud

Recommended for those who want to connect IoT endpoint devices and the cloud with low-power, low-cost systems and those who want to use AWS services.

In the future, the RL78/G23 (new product) evaluation board is also scheduled to receive FreeRTOS qualification and Renesas will contribute to the IoT of our customers, so please look forward to it.