New High-Accuracy Devices Enhance Reliability and Performance While Lowering Power Consumption of Memory Subsystems in Enterprise Computing Applications
2011年5月9日

SAN JOSE, Calif., May 9, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today introduced a new family of low-power, precision temperature sensors targeted at Double Data Rate 2 and 3 (DDR2 and DDR3) memory modules, Solid State Drives (SSD), and computing motherboards. These new devices complement IDT’s PCI Express®, signal integrity, flash memory controller, power management, and timing products to offer a rich set of application optimized enterprise computing solutions.

          The digital thermal sensors support both a 3.3V and lower-power 2.5V SM-Bus and I2C interface for improved system power efficiency and compatibility with both existing and emerging serial bus controllers. For further power savings, advanced on-die power management features minimize power consumption during critical modes, such as when mobile or fault-tolerant enterprise systems are operating on battery power. The new product family includes a stand-alone temperature sensor (TS3000GB2), as well as one with an integrated 256-byte EEPROM array (TSE2002GB2) on a single, monolithic die for non-volatile storage of user information, such as system configuration data for the Serial Presence Detect (SPD) feature of the memory module.

          The devices continue IDT’s tradition of industry-leading temperature accuracy by exceeding the requirements set forth by the Joint Electron Device Engineering Council (JEDEC) JC42.4 specification for Grade B temperature sensors, providing ±1°C temperature sensing accuracy over the entire temperature range of -20°C to +125°C. In addition, an innovative high-performance analog-to-digital converter (ADC) enables up to 12-bit (0.0625°C) programmable resolution with industry-leading conversion time, dramatically improving precision across the full temperature range.

          "Our customers are continually asking for increased system reliability and greater power efficiency, and IDT thermal sensors help us achieve these requirements,” said Arthur Sainio, Sr. Product Manager of SMART Modular Technologies. “We are pleased that IDT offers such a comprehensive portfolio of high-performance computing solutions to address the growing demand of the cloud computing market.”

          “As the next generation of computing equipment migrates to lower power and lower voltage architectures, IDT continues to lead those transitions with complete solutions for the memory module market,” said Mario Montana, vice president and general manager of the Enterprise Computing Division at IDT. “Our customers trust IDT to be a leader in performance, power and reliability, and our new family of thermal sensors reinforces that trust.”

          Both the TS3000GB2 and TSE2002GB2 support SM-Bus and I2C protocols and specifications, including timeout requirements critical for next generation systems, along with input glitch filtering and power-up voltage hysteresis to enhance fault tolerance in any customer system design.

Pricing and Availability
          The IDT temperature sensors are currently sampling to qualified customers. They are available in 8-pin DFN and TDFN packages that are RoHS compliant. The TSE2002GB2 and TS3000GB2 are priced at $0.85 and $0.75 each for volumes of 10,000 units, respectively. For additional information, visit
www.idt.com/go/TempSensor.

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com . Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.