electronica 2018: SOTB™ Energy Harvesting / Battery-less Agriculture Soil Monitor

The video explains an example of smart agriculture solution that uses Renesas’s SOTB Embedded Controller to realize maintenance-free with no requirement of replacing batteries. Power issue of smart agriculture solution is explained and the solution is given in the video, highlighting the benefit of SOTB technology and the capability of Energy Harvesting. SOTB realizes Energy Harvesting and brings innovation to smart agriculture applications.