QDRII+ Xtreme Devices Deliver Speeds of 633 MHz and up to 900 Million Random Transactions per Second, Enabling System Upgrade Without Re-Design

2011年4月20日

SAN JOSE and SANTA CLARA, Calif., April 20, 2011 — The QDR Consortium, which includes Cypress Semiconductor Corp. (NASDAQ:CY) and Renesas Electronics Corporation (TSE: 6723), today announced the industry's fastest Quad Data Rate (QDR) SRAM devices (static random access memory). The new memory devices will be named QDRII+ Xtreme and will operate at clock speeds as fast as 633 megahertz (MHz). They will be fit-, form- and function-compatible with existing QDR II+ devices, allowing manufacturers of network switches, routers and aggregation platforms to boost performance by simply increasing clock speeds within the system without any board design changes.

The new QDR II+ Xtreme SRAMs will be offered with either x18 or x36 word widths, and with bursts of 4 or 2 access. The burst of 4 devices delivers a random transaction rate (RTR) of 633 million random transactions per second, operating at clock speeds of 633 MHz, the highest available for a QDR SRAM. The burst of 2 offerings operate at a frequency of 450 MHz and offer an RTR of 900 million random transactions per second, which doubles the RTR of the prior generation burst of 4 devices running at the same frequency. The random transaction rate is defined as the number of fully random memory accesses per second and is the critical memory metric enabling increased line/switching rates.

“The QDR II+ Xtreme products provide a significant performance boost without requiring a system re-design, which is very appealing to networking equipment vendors looking to keep up with traffic demands,” said Dana Nazarian, Executive Vice President of the Memory Division at Cypress. “The QDR Consortium is actively defining a series of follow-on solutions which support the networking industry's ever-increasing memory requirements.”

“SRAM devices are another excellent option for customers who are seeking high-performance memory solutions,” said Hiroyuki Goto, senior manager, Industry & Network Business Division, Renesas Electronics Corporation. “We're pleased to stay on the forefront of SRAM technology with the QDR II+ Xtreme architecture.”

Availability

First engineering samples of the 36 megabit (Mb) and 72Mb QDR II+ Xtreme devices from Cypress are expected for lead customers in mid-2011.

About the QDR Consortium

The QDR Consortium was created in 1999 to define a new family of SRAM architectures for high-performance networking applications. QDR Consortium members cooperate in the development of the QDR family of networking SRAM devices. They design and manufacture this family of products in their own fabrication facilities and develop products according to their own schedules, competing in the marketplace. Additional information on the QDR SRAM technologies, including roadmaps, is available on our website at www.qdrconsortium.com.

QDR and Quad Data Rate SRAM devices comprise a family of products developed by Cypress and Renesas Electronics Corporation. All other trademarks are the property of their respective owners.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

この記事をシェアする