2018-06-22

The purpose of this 10-minute Out-of-Box (OOB) program illustrates a multithreaded application design that reads the analog values present on the potentiometer, light sensor and temperature sensor and displays those values on the included PMOD LCD Screen. The three LEDs on the board will flash or chase according to the value read from either the light sensor or the potentiometer. Switch 1 and Switch 2 are used to select which sensor is used and whether the LEDs flash or chase.