DRP-Accelerated Iris Detection and Extraction with Renesas RZ/A2M MPUs
Added on 6月 20, 2019
The DRP coprocessor accelerates iris detection and extraction for faster, more reliable authentication, enabled by pre-verified DRP libraries that enhance the video image, locate the subject’s irises, and capture cropped still images of each eye to be passed along to an iris-matching database. This is one of six demos Renesas Electronics presented at the Embedded Vision Summit 2019 in Santa Clara, CA, highlighting the capabilities of RZ/A and RZ/G MPUs for low-power, high-performance machine vision systems.