DRP-Accelerated Canny Edge Detection with Renesas RZ/A2M MPUs

Added on 6月 20, 2019

The DRP coprocessor accelerates Canny edge detection by more than 10 times compared to CPU-only processing in the RZ/A2M MPU. This is one of six demos Renesas Electronics presented at the Embedded Vision Summit 2019 in Santa Clara, CA, highlighting the capabilities of RZ/A and RZ/G MPUs for low-power, high-performance machine vision systems.