2018-06-22

This tutorial covers: registering with MyRenesas and logging in (required for download), accessing the RX compiler landing page, downloading the latest Renesas RX compilers We might want to make this version independent because updates are posted regularly, installing the compiler. This currently also still installs the HEW IDE which is a bit weird but just needs to be ignored by the users, starting e2studio afterwards and showing the easy Automatic Toolchain Detection feature (Installed RX and KPIT GNU toolchains (after v11.0x) are automatically detected and installed for use in e2studio when the product is launched).