Development Tools for Automotive Microcontrollers

IAR Systems Co., Ltd.

Functional safety measures are some of the most important features from recent years in embedded systems, especially the automotive, industrial and medical equipment areas.

By the way, did you know that the development tools used to develop your program is also included as part of the authentication process? If you did not receive an authentication for the development tools, then it is either the user will authenticate the tools before hand depending on the specialized and complex demands from the certification authority, or spend a lot of cost to consign it externally, and there is also a risk to be pushed to do the same before the antecedent (tool version) changes.

To resolve this issue, IAR Systems, as an integrated development environment with a compiler that has certified pre-functional safety standards, provides license packages for Renesas RX, RL78, and Arm® use.

The IAR Embedded Workbench functional safety version conforms to the international standards for functional safety IEC 61508, and the car automotive standard ISO 26262. It is also certified by the TÜV SÜD certification authority (TÜV Süd). In addition, the Arm® license has also obtained the European Railway Standard EN50128.

If the customer purchases the IAR system's functional safety version, they will be able to get continuous support from the certified build tool, the certification document and reports from TÜV SÜD, functional safety guidebook and compiler version fixation, thereby significantly reducing the time and cost spent on tool certification.

Added on 2018-05-12

The integrated development environment "IAR Embedded Workbench for RL78", as a micro-processor for low end use, is a tool that can fully demonstrate the capabilities of the RL78 Family with its processing power and low power consumption.

The loT Evaluation Kit is made up of the BLE wireless communication module, sensor, node, and device. This kit can be developed with the IAR Embedded Workbench for RL78. The kit also acts as a turn-key solution for the loT application development that makes use of RL78 micro-processor characteristics. Also, since the original Renesas in-house produced E1 emulator can be used in the debugging environment as is, additional costs can be reduced to a minimum while increasing the system's performance and efficiency.

The universal specification allows for switching the wireless communication BLE and Sub-GHz (920MHz), and the data that has been sensed can also be sent to and displayed on a tablet terminal. The sensor, node, and device included in the kit has a built-in speed sensor, temperature sensor and microphone. By using the sample code to immediately start it up, development time is shortened.

The IAR Embedded Workbench for RL78 uses its high compiler performance to produce even smaller and faster codes, making it the optimum development tool for applications that are strict on energy efficiency.

Added on 2018-05-11