Data Terminal Given Life with a Mirror

Renesas Electronics Corporation

The proximity sensor is given life with the application of capacitive touch keys. This is a demo of an equipment that can be operated without touching the touch keys since they detect hand gestures.
The mirror takes place of the terminal. When the target movement ends, it will return back to its mirror-like appearance.
If you hold your hand towards the half mirror, the Power On/Off, Alarm On/Off and LED dimming key appear.
You can adjust the LED’s brightness and make calls by controlling the keys with hand gesture depending on the situation.

 

*The mirror surface is actually a real one, but its dimmed for photography purposes.

Added on 2018-05-11