2021-09-07

This video shows you how to make Microsoft's Azure RTOS work on the RX65N Cloud Kit.
This is a tutorial on how to connect the RX65N Cloud Kit to the Azure IoT Hub and display the sensor data.
Have you set up your development environment yet?
If not, please refer to “Azure RTOS Tutorial (1/3)”.
This video is the program setup section. 
Firstly, the video explains the connection setup between the Azure IoT Hub and the RX65N Cloud Kit. Then, it shows how to set up the Azure connection information in the Azure RTOS sample code. Finally, it shows how to get connected to Azure IoT Hub after the build. This video will show you how to create these series of programs.

The sample code shown in the video can be downloaded from the following link.

* Previous Video

* Next Video