The CS Lab BACnet stack for RA MCUs helps developers save time and effort in the implementation of BACnet compatible applications. CS-Lab has compiled a library that supports programmers in the use of BACnet for a particular task (automation station). Routines of the BACnet stack take over the standard-compliant operation of the BACnet protocol, allowing the programmer to focus on the actual application.
User friendly, flexible, reliable
Many details are processed automatically so that users no longer have to worry about them. Thus, the functionality of the BACnet objects is implemented as an object database. In addition, various mechanisms and fallbacks for the value acquisition of field devices have been built into the code.