IDT RapidIO Switch Enables Texas Instruments to Build Scalable, High-Performance, Low-Power 4G Wireless Baseband Systems with Large Clusters of TMS320C6670 Digital Signal Processors
SAN JOSE, Calif., March 24, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that its IDT CPS-1616 RapidIO® Gen2 switch has been selected by Texas Instruments Incorporated (TI) for its new TMDXEVM6616 evaluation module (EVM). Now, designers can begin development on TI’s TCI6616 wireless base station System-on-Chip (SoC) for low latency, high performance and robust features to prototype 3G/4G wireless systems, significantly improving time to market. The inherent efficiency and software scalability of RapidIO in clustering large numbers of digital signal processors (DSPs) and Field Programmable Gate Arrays (FPGAs) on boards and over backplanes makes it the most effective interconnect choice for today’s wireless systems.
The IDT CPS-1616 belongs to IDT’s extensive portfolio of RapidIO Gen2 switches, supporting up to 20 Gbps per link for use as a chip-to-chip, board-to-board, and chassis-to-chassis interconnect. RapidIO enables OEMs in the 4G wireless and industrial markets to design embedded systems with clusters of DSPs that communicate in a peer-to-peer fashion while also providing high reliability, very low 100ns cut through latency, and simplified system memory maps. The use of RapidIO in TI’s TCI6616 EVM is a testament to the widespread adoption of the interconnect standard within the wireless infrastructure market.
"We’re incorporating IDT’s CPS-1616 RapidIO Gen2 switch on our EVM because of the scalability benefits it offers our customers,” said Kathy Brown, wireless base station infrastructure business manager, Texas Instruments. “We are now delivering the industry’s best and most mature RapidIO interfaces for interconnectivity across a broad portfolio of our wireless base station SoCs."
"We’re pleased that TI has selected IDT’s RapidIO switch for its wireless base station reference design” said Fred Zust, vice president of the Communications Division at IDT. “RapidIO is the ideal choice for clustering endpoints that require peer-to-peer communication, reliability, scalability, and high-performance in a single interconnect. Although there are several interfaces such as PCI Express and Gigabit Ethernet available on these DSPs and SoCs, customers continue to make use of RapidIO as the primary interconnect due to the advantages it offers. As a result, our customers can deploy smaller form factor base stations with more processing capacity in a more distributed network deployment model, delivering superior coverage, higher data rates and more services per 4G subscriber."
IDT’s rich portfolio of RapidIO products provides a wide selection of port and lane counts allowing customers to tailor their switch selection to the application. For more information about IDT’s RapidIO solutions, visit www.idt.com/go/S-RIO.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.