IDT Reduces Jitter by Over 50% Versus Competing Solutions and Offers the Industry’s First SyncE-compliant Solution that Meets the Most Stringent 10G or 40G Ethernet Performance Requirements

June 27, 2013

SAN JOSE, Calif., June 27,  2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the world’s lowest jitter ITU-T G.8262-compliant Synchronous Ethernet (SyncE) timing solutions. The new IDT 82V3910 is the first carrier-class SyncE-compliant phase-locked loop (PLL) device capable of meeting the most stringent 10G or 40G Ethernet PHY jitter performance requirements. With phase jitter below 300 femtoseconds (fs) RMS over the 10 kHz to 20 MHz integration range (with all channels in operation), this single-chip device offers 50 percent less jitter than competing solutions and replaces multichip alternatives to reduce design complexity and cost.

          The IDT 82V3910 and 82V3911 are low-jitter, highly-versatile SyncE network timing solutions optimized for use in 10GBASE-R/10GBASE-W and 40GBASE-R applications, including switches, routers, multiservice switching platforms, wireless backhaul equipment and other communications infrastructure. The innovative high-integration architecture includes two independent digital PLLs (DPLLs) to allow bidirectional synchronization for maximum utility and simplified deployment. The DPLLs lock to a wide variety of telecom and Ethernet reference frequencies and suppress incoming timing faults to generate highly-reliable output clocks for optimal network performance.

          “Our latest SyncE network timing devices combine IDT’s industry-leading digital and analog PLL technologies to achieve the first integrated synchronization solution addressing the large and fast-growing market for 10G and 40G applications,” said Christian Kermarrec, vice president and general manager of the Timing and Synchronization Division at IDT. “With jitter less than half that of competing products, the new clocking solutions offer our customers the ultimate in performance and versatility by supporting the most stringent low-jitter requirements found in 10G or 40G Ethernet applications. These devices complement IDT’s rich timing portfolio, including RF and network PLLs, VCXOs, synthesizers, buffers, frequency translators and crystal oscillator replacement products.”

          The IDT 82V3910 SyncE SETS simplifies the timing circuit and bill-of-materials (BOM) by providing the synchronous equipment timing source (SETS) function to manage all required synchronization timing signals. Ultra-low jitter generation makes the 82V3910 particularly suitable for single-board systems where the SETS directly times 10G or 40G network PHYs. The 82V3910 complies with ITU-T G.8262 for EEC-Options 1 and 2; and G.813 for SEC-Options 1 and 2; and is suitable for SyncE, SONET and SDH equipment. The 82V3910 can synchronize directly to a one pulse per second (1 PPS) reference enabling the host system to use a low-cost GPS receiver.

          The single-chip 82V3911 SyncE PLL is pre-engineered to select references from a variety of SETS or network sources, perform clock rate conversions, and attenuate jitter – all while preserving the G.8262 compliance of the selected references. Furthermore, the 82V3911 reduces timing circuit BOM cost and board space by providing two PLL channels in a single chip.

Pricing and Availability
          The IDT 82V3910 and 82V3911 are available now and are encapsulated in a 196-ball 15 x 15 mm CABGA Package. The IDT 82V3910 and 82V3911 are priced at $35.20 and $25.50 each for volumes of 1,000 units, respectively. For more information about IDT’s leading clock ICs and timing solutions, please visit www.idt.com/go/timing.

About IDT Clock and Timing Solutions
          With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. IDT has also expanded its portfolio to include frequency control products, such as the XpressO® oscillators from Fox Electronics and an innovative line of MEMS oscillators that are rapidly replacing legacy quartz-based oscillators. For more information about IDT’s leading portfolio of timing products, please visit www.idt.com/go/timing.

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world, with direct purchase services through IDT Direct™. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on

Share this news on