IDT’s Single-chip Wireless Power IC Offers Mobile OEMs Seamless Compatibility Between the Latest Versions of Two Popular Magnetic Induction Wireless Charging Standards
SAN JOSE, Calif., February 24, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced the industry’s first dual-mode wireless power receiver compatible with both the Wireless Power Consortium’s (WPC) 1.1 Qi standard, as well as the Power Matter’s Alliance (PMA) 1.1 standard. The innovative solution enables OEMs to use a single wireless power receiver IC to develop mobile devices fully compatible with the latest versions of both Qi and PMA charging bases.
The IDTP9023 is a WPC 1.1- and PMA 1.1-compliant single-chip wireless power receiver consisting of a synchronous full-bridge rectifier, high-efficiency synchronous buck converter, and embedded microcontroller used to optimize power delivery to the mobile device’s load, while minimizing application footprint, component count, and thermal dissipation. The new wireless power receiver supports all WPC and PMA receiver coils, as well as proprietary and PCB-based coils for maximum versatility in a wide range of applications, including smart phones, tablets, sleeves, and other accessories.
“We are proud to continue our wireless power technology leadership by announcing the industry’s first single-chip WPC 1.1 and PMA 1.1 dual-mode wireless power receiver solution,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “Following the industry’s first dual-mode solution IDT announced last year, our new device gives customers a clear upgrade path to meet the latest magnetic induction standards requirements and offer consumers full compatibility with any Qi- or PMA-certified charging base currently on the market. The chip’s high-efficiency and small application footprint make it well-suited for tomorrow’s ultra-thin, lightweight, and compact portable devices and accessories.”
The embedded microcontroller provides a variety of control features and status indicators beyond the Qi and PMA specifications, enabling the development of sophisticated power delivery schemes and innovative user interfaces. Enhanced communication with IDT’s wireless power transmitters is achieved via a proprietary transmitter/receiver back-channel communication protocol, while an integrated I2C interface provides access to charging status and proprietary alignment guide information.
In addition, flexible firmware and microcontroller programmability enables tuning the coil drive circuitry to maximize power transfer efficiency for various applications and usage scenarios. With excellent power efficiency and compliance to the latest WPC and PMA standards, the device offers a quick battery charge with any Qi- or PMA-compatible charging base. For applications not requiring dual-mode capability, a Qi-only version is available as the IDTP9022.
Customers who are considering adding wireless charging capability to their electronic devices are encouraged to watch informational videos and download technical documentation at www.wirelesspowerbyidt.com.
Availability
The IDTP9023 and IDTP9022 are currently sampling to qualified customers and are available in a compact 3.9 x 4.1 mm WLCSP package. For more information about IDT’s leading inductive charging and magnetic resonance solutions, please visit www.wirelesspowerbyidt.com or contact your local IDT sales representative.
About IDT Wireless Power
IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member. IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.
About IDT
Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.
###
IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.