IDT Expands Leading Wireless Power Portfolio with High-efficiency Solution Offering Full WPC 1.1-compliance for Smartphones, Tablets, and Accessories

October 28, 2013

SAN JOSE, Calif., October 28, 2013 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced a new wireless power receiver meeting the Wireless Power Consortium’s (WPC) 1.1 “Qi” specification and optimized for high-volume portable consumer applications. The new device expands upon IDT’s award-winning wireless power family, offering portable device manufacturers a high-efficiency, cost-effective wireless power solution for universal compatibility with the next-generation of Qi charging bases.

          The IDTP9025 is a single-chip wireless power receiver IC certified to meet the requirements of the WPC 1.1 specification, offering improved foreign object detection (FOD) compared to earlier versions of the standard. The highly-integrated device includes an onboard synchronous full-bridge rectifier and low-resistance low-dropout (LDO) regulator, enabling customers to achieve excellent power transfer efficiency with minimal external component count and board space. The high-efficiency, cost-effective design is ideal for use in high-volume portable devices where battery life and physical size are a primary concern, such as in smartphones, tablets, and related accessories.

          “Our latest WPC 1.1 wireless power receiver expands our leading wireless power portfolio to address high-volume portable consumer products,” said Arman Naghavi, vice president and general manager of the Analog and Power Division at IDT. “The IDTP9025 enables our customers to develop compact, high-efficiency wireless power solutions compliant to the latest standards, ensuring universal compatibility with any Qi charging base. We also provide a WPC 1.1-certified reference design and layout guidelines with our evaluation kits, making it easy for our customers to obtain WPC certification for their products with minimal effort.”

          For added control, IDTP9025 is capable of passing communication and power transfer information to a local microcontroller, as well as fault and safety monitors, through the integrated I2C port. This allows the customer to build custom control algorithms and user interfaces to enhance the user experience. In addition to an evaluation kit with WPC-certified reference design, IDT supports its customers with a design-in guide and powerful support tools to further ease the development process.

Availability
          The IDTP9025 is currently sampling to qualified customers and is available in a compact 3 x 2.5 mm WLCSP package. The IDTP9025 part number is priced at $2.44 each for volumes of 1,000 units. For more information about IDT’s industry-leading wireless power ICs, visit www.wirelesspowerbyidt.com.

About IDT Wireless Power

          IDT is a leader in wireless power transmitter and receiver solutions for wireless charger applications, addressing all major standards and technologies with an extensive portfolio of standards-certified products. IDT has proven expertise in both magnetic induction and magnetic resonance technologies, and actively participates in the Wireless Power Consortium (WPC), Power Matters Alliance (PMA), and Alliance for Wireless Power (A4WP) as a board member.  IDT has introduced a number of innovative and award-winning products, including the first true single-chip transmitter, the highest-output-power single chip receiver, and the first dual-mode receiver IC compatible with both WPC and PMA standards. Prominent industry players have recognized this leadership and partnered with IDT as their silicon vendor for next-generation wireless power solutions.

About IDT

          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.