IDT’s SoC-friendly Ultra-low Power PCIe Buffers Use the Same 1.5 V Voltage Rail as Modern SoCs, Reducing System Complexity, Size, and Power

July 23, 2014

SAN JOSE, Calif., July 23, 2014 – Integrated Device Technology, Inc. (IDT®) (NASDAQ: IDTI) today announced the expansion of its leading PCIe timing portfolio with the industry’s first 1.5 V PCI Express (PCIe®) buffer family. IDT’s new U-series ultra-low power PCIe buffers operate from the same supply voltage as modern systems-on-chip (SoCs) and field programmable gate arrays (FPGAs), enabling designers to use the same power rail, thus reducing system complexity, physical size, and power consumption.

The 9DBU buffers are offered in 2 to 9-output configurations to address virtually any PCIe application. Both non-PLL fan out and PLL zero-delay-buffer modes are supported.

“IDT has consistently led the timing industry in both performance and power, and the latest family of devices furthers our leadership position,” said Dave Shepard, vice president and general manager of Timing and RF at IDT. “SoCs and FPGAs are moving to lower supply voltages and IDT is extending its PCIe timing solutions portfolio to address this trend. Our 1.5 V solutions take advantage of the low-voltage power savings, while simultaneously enabling customers to consolidate power rails to reduce the complexity of their systems. The new timing solutions complement IDT’s V-series of 1.8 V PCIe clocks for communications, computing, and consumer markets.”

Device options include external or internal terminations, allowing designers to choose between maximum flexibility with external termination circuitry, or maximum space savings using internal terminations. The entire family operates from a 1.5 V supply, resulting in the industry’s lowest power consumption for PCIe timing devices, with eight-output devices using a mere 40 milliwatts – reducing cooling requirements and lowering operating costs.

The 1.5 V U-series devices are pin-compatible with IDT’s widely-adopted 1.8 V V-series, allowing for easy substitution as SoC operating voltages continue to drop. The 9DBU buffers are compliant with PCIe Gen 1, 2, and 3 so designers can use the same component through several generations of product.

Pricing and Availability

The IDT 9DBU buffers are currently sampling to qualified customers. They are available in standard VFQFPN packages ranging from 4 x 4 mm to 6 x 6 mm. Please contact your local sales representative or distributor for pricing and availability. For more information about IDT’s rich portfolio of PCI Express solutions, visit www.idt.com/go/PCIe.

About IDT Clock and Timing Solutions

With a product portfolio 10 times greater and broader than any other, IDT is the world’s leader in silicon timing and is in a unique position to address the needs of virtually any application. With the industry’s largest market share, IDT is the only one-stop-shop for timing, offering products from full-featured system solutions to simple clock building-block devices. Factory-programmable options and clock solution customization capabilities address unique customer requirements, while the lowest jitter and lowest power features set IDT apart from the competition. Products are accompanied by a world-class support team driven by service and responsiveness goals. IDT has also expanded its portfolio to include frequency control products, such as the XpressO® oscillators from Fox Electronics®. For more information about IDT’s leading portfolio of timing products, please visit www.idt.com/go/timing.

About IDT

Integrated Device Technology, Inc. develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing, sales facilities and distribution partners throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.

Share this news on

Share this news on