IDT’s Latest Wide Area Network (WAN) Phase-Locked Loop (PLL) Supports Both Synchronous Ethernet and IEEE 1588 Applications for Cloud Computing and 4G Telecom Infrastructure

December 7, 2011

SAN JOSE, Calif., December 7, 2011 – Integrated Device Technology, Inc. (IDT®; NASDAQ: IDTI), the Analog and Digital Company™ delivering essential mixed-signal semiconductor solutions, today announced that it has expanded its leading timing portfolio with the industry’s most versatile WAN PLL supporting both Synchronous Ethernet (Sync Ethernet) and IEEE 1588 applications in cloud-based networking and 4G wireless infrastructure.

          The IDT82V3391 is an integrated, single-chip PLL that supports both Sync Ethernet and IEEE1588 with legacy support for SDH, Sonet and T1/E1 clock rates. The broad range of supported protocols makes this product highly versatile, allowing system designers to use a single PLL device to support a wide range of applications. In addition, the device is capable of synchronizing to a 1 pulse-per-second (pps) input signal while simultaneously providing a 1 pps output, a feature that has become popular with 4G and LTE technologies. Ultimately, the extreme flexibility of IDT’s new PLL helps customers simplify their bill of materials (BOM) and reduce the total cost of their systems.

          “As the world leader in silicon timing, we actively maintain the industry’s broadest portfolio of innovative devices,” said Fred Zust, general manager and vice president of the Communications Division at IDT. “The complexity of communication hardware is growing exponentially, so we work to simplify it by developing advanced ICs. The latest addition to our family of WAN PLLs provides our customers with the flexibility and performance they require for their next-generation cloud-based networking and 4G wireless infrastructure applications.”

          The device’s support for the Sync Ethernet standard is a key feature, as this standard has become popular in networking as a low-cost alternative to SONET/SDH. Likewise, the IEEE 1588 standard has gained in popularity, allowing customers to optimize network performance via delay measurement though the network. In both cases, an accurate timing reference is critical to maintaining high-performance network operation. IDT’s new PLL exceeds the stringent requirements of these standards with low phase noise and an impressive accuracy of 0.011 parts per billion.

Availability
The IDT82V3391 is currently sampling to qualified customers and is available in a 100-pin thin quad flat pack (TQFP) package. For more information about IDT’s extensive clock and timing portfolio, visit
www.idt.com/go/WAN-PLL .

About IDT
          Integrated Device Technology, Inc., the Analog and Digital Company™, develops system-level solutions that optimize its customers’ applications. IDT uses its market leadership in timing, serial switching and interfaces, and adds analog and system expertise to provide complete application-optimized, mixed-signal solutions for the communications, computing and consumer segments. Headquartered in San Jose, Calif., IDT has design, manufacturing and sales facilities throughout the world. IDT stock is traded on the NASDAQ Global Select Stock Market® under the symbol “IDTI.” Additional information about IDT is accessible at www.IDT.com. Follow IDT on Facebook, LinkedIn, Twitter, and YouTube.

###

IDT and the IDT logo are trademarks or registered trademarks of Integrated Device Technology, Inc. All other brands, product names and marks are or may be trademarks or registered trademarks used to identify products or services of their respective owners.