Contributes to More Compact Inverter Systems for Applications such as Industrial Machinery and Solar Power Systems

January 31, 2013

TOKYO, Japan, January 31, 2013 — Renesas Electronics Corporation (TSE: 6723), a premier supplier of advanced semiconductor solutions, today announced two new photocouplers PS9332L and PS9332L2, with an integrated insulated-gate bipolar transistor (IGBT) (Note 1) protection function, for applications such as industrial machinery and solar power systems.

The new PS9332L and PS9332L2 feature an integrated active Miller clamp circuit (Note 2) to prevent IGBT malfunction, world-top-class high-speed switching (20 percent faster than conventional Renesas products) among IGBT drive photocouplers with integrated IGBT protection function, compact 8-pin SDIP (shrink dual inline package), and guaranteed high-temperature operation. The photocouplers can be used for gate drive of IGBT devices used in inverter circuits for motor control, etc.

It is common to protect a circuit such as an inverter with insulating devices such as couplers when dealing with comparably high voltages.

A photocoupler combines in a single package a light emitting diode (LED) on the input side, to convert an electrical signal into light, and a photo detector on the output side, to convert the light into an electrical signal. The input and output sides are electrically isolated from each other because the signal is conveyed between them in the form of light. Types of photocouplers include general-purpose photocouplers (transistor output) for applications such as power supply, and IGBT drive photocouplers, which are used for gate drive of IGBT devices in applications such as solar power generators or general-purpose inverters.

The new PS9332L and PS9332L2 are IGBT drive photocouplers consisting of a gallium-aluminum-arsenide (GaAlAs) LED as the light emitting diode, photo detector IC, and an IGBT protection circuit. They are designed to drive the gate of an IGBT device while at the same time providing an integrated protection function (active Miller clamp) to prevent destruction due to malfunction of the IGBT. In a conventional system this protection function must be implemented by means of external components, resulting in a more complex system design and making miniaturization difficult. The new PS9332L and PS9332L2 solve this problem.

Key Features of the New Photocoupler PS9332L and PS9332L2:

(1) On-chip active Miller clamp circuit to prevent IGBT malfunction

When the IGBT connected to the photocoupler turns off, current flow (Miller current) between the collector and gate can cause a gate voltage, resulting in malfunction. The integrated active Miller clamp circuit shortens the gate charge to ground, suppressing any rise in the gate voltage and preventing malfunction. Integrating the protection circuit into the photocoupler simplifies system design and enables the system to be more compact overall.

(2) The highest speed level of switching (20 percent faster than conventional Renesas products)

The photo detector IC uses Renesas' exclusive BiCMOS process, resulting in low parasitic capacitance (Note 3), shorter delay time (tPHL, tPLH ≤ 200 ns, 20 percent less than comparable earlier products), and low current consumption by the circuit (Icc ≤ 2.5 mA). This makes it possible to build inverter control circuits that are more precise and have lower power consumption. In addition, the circuit's low current consumption enables a more compact power supply for the system driving the IGBTs.

(3) Compact 8-pin SDIP package

Although it now includes an integrated active Miller clamp function, the size of the photo detector chip is equivalent to that of comparable earlier products, allowing a compact 8-pin SDIP package. This provides a 40 percent reduction in mounting area compared with an 8-pin DIP, allowing customers to build more compact systems.

The package is available with two lead frame options. The PS9332L offers 7 mm outer creepage, whereas the PS9332L2 offers 8 mm.

(4) Guaranteed high-temperature operation

The materials have been improved to allow operation at high temperatures, for a maximum operating ambient temperature of 125 degrees C. This simplifies the thermal design of systems in hot environments.

Renesas believes the new PS9332L and PS9332L2 will simplify development of and allow greater compactness in inverter products, the market for which is expected to grow moving forward. While expanding sales promotion aggressively, Renesas will continue to develop new products with support for the high-temperature, high-speed, and high-output requirements of customers.

Using the new products in combination with Renesas' IGBT can reduce dead time in switching by about 10 percent (compared with conventional Renesas products) and improve power efficiency. Also, Renesas expands support of customers’ product development with reference boards for devices such as power conditioners and inverters as kit solution with MCUs.

(Note 1 Insulated-gate bipolar transistors are used in high-voltage, large-current switching applications.

(Note 2) A circuit that absorbs the ineffective current (mirror current) generated via the parasitic capacitance between the collector and gate of an IGBT.

(Note 3) Unwanted capacitance components that are generated due to the physical characteristics of the interior of the chip. Also called floating capacitance.

Refer to the separate sheet for the main specifications of the PS9332L and PS9332L2.

Pricing and Availability

Samples of the new PS9332L and PS9332L2 will start in February 2013, priced at US$2.00 per unit. Mass production of the PS9332L and PS9332L2 is scheduled to begin around June 2013 and is expected to reach a scale of 1,000,000 units per month in October 2013. (Pricing and availability are subject to change without notice.)

(Remarks)
All other registered trademarks or trademarks are the property of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.

Share this news on