Renesas Electronics Introduces New V850 Microcontroller (MCU) Series with Very Low Power Consumption and High Functionality for Body Applications in the Automotive Segment

14 Feb 2012

TOKYO, Japan, February 14, 2012 — Renesas Electronics Corporation (TSE: 6723), a premier provider of advanced semiconductor solutions, today announced the development of the V850E2/Fx4-L series with 19 new 32-bit microcontrollers (MCUs). Designed for the automotive comfort and body segment, the low-power MCUs offer scalability and compatibility combined with sophisticated peripheral functions to provide premium automotive body solutions for applications such as roof or window lifters, door-, seat- and light modules, HVAC (heating, ventilation, and air conditioning) and body control modules.

 

The new V850-based MCU series enables very low current consumption in active mode of less than 0.35 milliamps (mA) at 1 megahertz (MHz).

 

The V850E2/Fx4-L MCUs provide a unique power-saving feature called the sequencer (SEQ). The SEQ supports hardware monitoring of digital inputs in deep stop mode without any usage of the CPU or memory. When the SEQ detects activities at the digital inputs, the device switches from deep stop mode to run mode. A further unique feature is the LIN-master controller (LMA) which supports the automatic LIN-frame detection without CPU interactivity.

 

The new, low-power V850E2/Fx4-L MCUs combine and extend the legacy technologies of the two merged companies, NEC Electronics and Renesas Technology: the V850 32-bit RISC CPU and the power-saving MONOS (metal oxide nitride oxide silicon) flash technology employing 90-nanometer (nm) process technology of the RX and SH™ MCU Families.

  

The V850E2/Fx4-L MCUs incorporate a maximum CPU clock from 48 MHz up to 64 MHz with a performance of 1.81 Dhrystone MIPS (DMIPS)/MHz. With the adoption of AUTOSAR and increased system functionality, there is growing demand for larger memory capacity. The V850E2/Fx4-L MCUs address this demand by providing flash memory ranges from 256 kilobytes (KB) up to 1.5 megabytes (MB) equipped in packages with pin counts ranging from 64 to 176. An enhanced peripheral set is implemented, including PWM generation, up to two CAN interfaces as well as 8 DMA (direct memory access) channels. 

 

Fully-verified AUTOSAR MCAL (microcontroller abstraction layer) software drivers are scheduled to be prepared. Renesas' MCAL software drivers can be obtained as a stand-alone software package or integrated in a complete basic software stack in cooperation with partner companies. To comply with the AUTOSAR requirements, new system protection functionality (SPF) has been implemented in all V850E2/Fx4-L devices. The SPF includes a memory protection unit (MPU) and a system register protection (SRP).

 

Refer to the separate sheet for the main specifications of the V850E2/Fx4-L MCUs.

 

Pricing and Availability

Samples of Renesas' new V850E2/Fx4-L MCUs are available now priced at US$20 per unit. Mass production is scheduled to begin in the beginning of CY2013 and is expected to reach a volume of 1,500,000 units per month in December 2013. (Pricing and availability are subject to change without notice.)

 

Exhibition at Embedded World 2012

Renesas' V850E2/Fx4-L MCUs will be showcased at Embedded World 2012, to be held in Nuremberg, Germany from February 28 to March 1, 2012.

(Remarks) SuperH is a trademark or registered trademark of Renesas Electronics Corporation in Japan, the USA, and other countries. All registered trademarks or trademarks are the property of their respective owners.

About Renesas Electronics Corporation

Renesas Electronics Corporation (TSE: 6723) delivers trusted embedded design innovation with complete semiconductor solutions that enable billions of connected, intelligent devices to enhance the way people work and live. A global leader in microcontrollers, analog, power, and SoC products, Renesas provides comprehensive solutions for a broad range of automotive, industrial, infrastructure, and IoT applications that help shape a limitless future. Learn more at renesas.com. Follow us on LinkedIn, Facebook, Twitter, and YouTube.


The content in the press release, including, but not limited to, product prices and specifications, is based on the information as of the date indicated on the document, but may be subject to change without prior notice.